Skip to main content
RSing.17
Associate II
May 5, 2023
Question

How to interface STM32f767zit6 with ethernet rotary encoder using ethernet communication?

Hello, I wanted to interface and get the readings from ethernet/IP encoder from Fraba with stm32767zit6. Is there any way to communicate it stm32f767zit6 and get the data from the encoder.

PS- Below is the datasheet of the absolute rotary encoder which I am using.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 5, 2023

Related / Dupe ​https://community.st.com/s/question/0D53W00002FbMg7SAF/can-anyone-help-me-interface-my-stm32f767zit6-board-with-ethernet-with-detailed-explanation

​

What board do you have, you mention a chip, do you have the NUCLEO board, or something else?

​

E​xpect to have to read the specifications and implement a TCP/IP protocol stack so you can send / receive packets

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RSing.17
RSing.17Author
Associate II
May 5, 2023

The board is stm32f767zit6 NUCLEO