Skip to main content
ADing.1
Associate II
Apr 3, 2023 6:45 PM UTC
Solved

LPM01A cannot connect to STM32CubeMonitor-Power

I downloaded Cube Power Monitor and am trying to use it to connect to the LPM01A. I have downloaded and installed the W8 version of the virtual com port driver.

I can select the board in the drop down menu, but when I hit "Take Control", a dialog box pops up with the message `error pwr get`. When I hit okay, another pops up with the message `Get current range command failed` with another message below it `ERROR TIMEOUT`. Hitting ok again gives yet another dialog box with the message `Board has been released due to connection issue. Please unplug and plug the board`.

I've tried unplugging and plugging it back in and the same thing happens. I am currently on Windows 11, but I've tried on a different windows 10 machine and the result was exactly the same.

Any help would be appreciated.

Please also take a look at my other question for something that might be related... having lots of issues with this board so far...

This topic has been closed for replies.
FM.1
FM.1Best answer
Associate
Apr 28, 2023 8:03 PM UTC

I confirm it works now on Ubuntu 22.04 with 1.2.0 after updating the lpm01a board (from 1.0.1) to 1.0.8 (the latest at the time of writing).

11 replies

ADing.1
ADing.1Author
Associate II
Apr 3, 2023 9:21 PM UTC

Figured out a solution...

If I use version 1.1.1 instead of 1.2.0, then it works ... :expressionless_face:

HMaka.3
Visitor II
Apr 10, 2023 11:50 AM UTC

Same behaviour

Richard.Chvr
ST Technical Moderator
Apr 6, 2023 8:04 AM UTC

@PDEFO.1​, can you have a look

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PDEFO.1
ST Employee
Apr 6, 2023 8:12 AM UTC

Thanks for your question. This issue was not reported before and not observed during validation tests.

For such issue it would be helpfull to get a log. Logs of the tool is located here :

C:\Users\<username>\AppData\Local\Temp\Power_Monitor\Logs

FM.1
Associate
Apr 26, 2023 7:24 PM UTC

Where can I find the logs on Ubuntu 22.04?

PDEFO.1
ST Employee
Apr 27, 2023 7:27 AM UTC

Logs for Linux are located In the "java temp directory"/powermonitor

FM.1
FM.1Best answer
Associate
Apr 28, 2023 8:03 PM UTC

I confirm it works now on Ubuntu 22.04 with 1.2.0 after updating the lpm01a board (from 1.0.1) to 1.0.8 (the latest at the time of writing).

Richard.Chvr
ST Technical Moderator
Mar 6, 2025 1:12 PM UTC

Hello @PPa

Can you give more details about the STM32PowerMonitor errors.

Which version of STM32-LPM01-XN firmware are you using? You may updated in following link.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.