Skip to main content
KRott.1
Associate
Feb 15, 2023 7:59 PM UTC
Solved

Incorrect interrupt firing for stm32f4 CAN2

I have not been able to get CAN2_RX0_IRQ or CAN3_RX0_IRQ to fire. CAN1_RX0_IRQ works as expected. It appears that rather than the CAN IRQs firing, the WWDG interrupt is going off for CAN2_RX0 and the DMA1_Stream0 is going off for CAN3_RX0. Neither the WWDG or the DMA1_Stream0 interrupts are enabled. I was able to figure this out because CAN1 works as long as you do not connect anything to CAN2 or CAN3. If you plug other nodes into either of those CAN busses the mcu would die at the other interrupt handlers. After messing with the CAN initialization and filters for days, I decided to just try calling HAL_CAN_IRQHandler from the improper interrupt handler and sure enough I have communication working on all three can busses. The vector table start has been placed at 0x8060100. Below you can see that I have disassembled the addresses for the IRQ's in question. They all make a call to HAL_CAN_IRQHandler that then calls the FIFO0PendingCallback where we read in the CAN messages, but the CAN interrupt handlers are never called. All of this has led me to believe this is an actual hardware problem or a micro code issue that is looking up the incorrect interrupt. I have already considered that the vector offset was messed up, but the CAN1 interrupts have never stopped working.

loactions of irqs according to the user manual

WWDG 0x00000040

Dma1_Stream0 0x0000006c

CAN2_RX0 0x00000140

CAN3_RX0 0x0000016c

(gdb) disassemble *0x8060140

Dump of assembler code for function Hal::WWDG_IRQHandler():

  0x0807fbd8 <+0>:   push   {r7, lr}

  0x0807fbda <+2>:   add   r7, sp, #0

  0x0807fbdc <+4>:   mov.w   r1, #296   ; 0x128

  0x0807fbe0 <+8>:   ldr   r0, [pc, #24]   ; (0x807fbfc <Hal::WWDG_IRQHandler()+36>)

  0x0807fbe2 <+10>:   bl   0x80cec30 <printf>

  0x0807fbe6 <+14>:   movs   r1, #1

  0x0807fbe8 <+16>:   ldr   r0, [pc, #20]   ; (0x807fc00 <Hal::WWDG_IRQHandler()+40>)

  0x0807fbea <+18>:   bl   0x807fd50 <std::array<__CAN_HandleTypeDef, 3u>::operator[](unsigned int)>

  0x0807fbee <+22>:   mov   r3, r0

  0x0807fbf0 <+24>:   mov   r0, r3

  0x0807fbf2 <+26>:   bl   0x8083a5a <HAL_CAN_IRQHandler>

  0x0807fbf6 <+30>:   nop

  0x0807fbf8 <+32>:   pop   {r7, pc}

  0x0807fbfa <+34>:   nop

  0x0807fbfc <+36>:   ldr   r0, [r4, #20]

  0x0807fbfe <+38>:   lsrs   r5, r1, #32

  0x0807fc00 <+40>:   lsls   r0, r4, #25

  0x0807fc02 <+42>:   movs   r0, #0

End of assembler dump.

(gdb) disassemble *0x806016c

Dump of assembler code for function Hal::DMA1_Stream0_IRQHandler():

  0x0807fc68 <+0>:   push   {r7, lr}

  0x0807fc6a <+2>:   add   r7, sp, #0

  0x0807fc6c <+4>:   movw   r1, #333   ; 0x14d

  0x0807fc70 <+8>:   ldr   r0, [pc, #24]   ; (0x807fc8c <Hal::DMA1_Stream0_IRQHandler()+36>)

  0x0807fc72 <+10>:   bl   0x80cec30 <printf>

  0x0807fc76 <+14>:   movs   r1, #2

  0x0807fc78 <+16>:   ldr   r0, [pc, #20]   ; (0x807fc90 <Hal::DMA1_Stream0_IRQHandler()+40>)

  0x0807fc7a <+18>:   bl   0x807fd50 <std::array<__CAN_HandleTypeDef, 3u>::operator[](unsigned int)>

  0x0807fc7e <+22>:   mov   r3, r0

  0x0807fc80 <+24>:   mov   r0, r3

  0x0807fc82 <+26>:   bl   0x8083a5a <HAL_CAN_IRQHandler>

  0x0807fc86 <+30>:   nop

  0x0807fc88 <+32>:   pop   {r7, pc}

  0x0807fc8a <+34>:   nop

  0x0807fc8c <+36>:   ldr   r0, [r4, #20]

  0x0807fc8e <+38>:   lsrs   r5, r1, #32

  0x0807fc90 <+40>:   lsls   r0, r4, #25

  0x0807fc92 <+42>:   movs   r0, #0

End of assembler dump.

(gdb) disassemble *0x8060240

Dump of assembler code for function Hal::CAN2_RX0_IRQHandler():

  0x0807fc04 <+0>:   push   {r7, lr}

  0x0807fc06 <+2>:   add   r7, sp, #0

  0x0807fc08 <+4>:   movs   r1, #1

  0x0807fc0a <+6>:   ldr   r0, [pc, #16]   ; (0x807fc1c <Hal::CAN2_RX0_IRQHandler()+24>)

  0x0807fc0c <+8>:   bl   0x807fd50 <std::array<__CAN_HandleTypeDef, 3u>::operator[](unsigned int)>

  0x0807fc10 <+12>:   mov   r3, r0

  0x0807fc12 <+14>:   mov   r0, r3

  0x0807fc14 <+16>:   bl   0x8083a5a <HAL_CAN_IRQHandler>

  0x0807fc18 <+20>:   nop

  0x0807fc1a <+22>:   pop   {r7, pc}

  0x0807fc1c <+24>:   lsls   r0, r4, #25

  0x0807fc1e <+26>:   movs   r0, #0

End of assembler dump.

(gdb) disassemble *0x806026c

Dump of assembler code for function Hal::CAN3_RX0_IRQHandler():

  0x0807fc3c <+0>:   push   {r7, lr}

  0x0807fc3e <+2>:   add   r7, sp, #0

  0x0807fc40 <+4>:   movw   r1, #327   ; 0x147

  0x0807fc44 <+8>:   ldr   r0, [pc, #24]   ; (0x807fc60 <Hal::CAN3_RX0_IRQHandler()+36>)

  0x0807fc46 <+10>:   bl   0x80cec30 <printf>

  0x0807fc4a <+14>:   movs   r1, #2

  0x0807fc4c <+16>:   ldr   r0, [pc, #20]   ; (0x807fc64 <Hal::CAN3_RX0_IRQHandler()+40>)

  0x0807fc4e <+18>:   bl   0x807fd50 <std::array<__CAN_HandleTypeDef, 3u>::operator[](unsigned int)>

  0x0807fc52 <+22>:   mov   r3, r0

  0x0807fc54 <+24>:   mov   r0, r3

  0x0807fc56 <+26>:   bl   0x8083a5a <HAL_CAN_IRQHandler>

  0x0807fc5a <+30>:   nop

  0x0807fc5c <+32>:   pop   {r7, pc}

  0x0807fc5e <+34>:   nop

  0x0807fc60 <+36>:   ldr   r0, [r4, #20]

  0x0807fc62 <+38>:   lsrs   r5, r1, #32

  0x0807fc64 <+40>:   lsls   r0, r4, #25

  0x0807fc66 <+42>:   movs   r0, #0

This topic has been closed for replies.
KRott.1
KRott.1Best answer
Associate
Feb 17, 2023 9:23 PM UTC

wow, thanks @Community member​ that seems to have fixed our problem. Vector table is now located at 0x8060200

4 replies

S.Ma
Principal
Feb 16, 2023 6:32 AM UTC

I had wrong interrupt firering experience when the interrupt vector table was missing few vectors and some were shifted... this is something to check in the startup .s file.

KRott.1
KRott.1Author
Associate
Feb 16, 2023 2:23 PM UTC

@S.Ma​  thanks, i did check the whole table and it matches the order in the manual, I made sure the reserved spaces were all there as well.

waclawek.jan
Super User
Feb 17, 2023 5:37 PM UTC

> The vector table start has been placed at 0x8060100

You have to align VTOR to the size of vector table rounded up to nearest power of two, i.e. here at 0x200 boundary.

JW

KRott.1
KRott.1AuthorBest answer
Associate
Feb 17, 2023 9:23 PM UTC

wow, thanks @Community member​ that seems to have fixed our problem. Vector table is now located at 0x8060200