Skip to main content
DS.4
Senior
Jan 29, 2023 10:09 AM UTC
Question

Target is not responding, retrying...

Using a sample example from your database code.

Compatible with stack 1.15.0 (that is the stack I am running)

STMicroelectronics ST-LINK GDB server. Version 7.1.0

Copyright (c) 2022, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.12.0          

   -------------------------------------------------------------------

Log output file:  C:\Users\NOVODES\AppData\Local\Temp\STM32CubeProgrammer_a01928.log

ST-LINK SN : 066DFF505655806687075314

ST-LINK FW : V2J40M27

Board    : P-NUCLEO-WB55

Voltage   : 3.27V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x495

Revision ID : Rev Y

Device name : STM32WB5x/35xx

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xD5

Debug in Low Power mode enabled

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a01928.srec

 File     : ST-LINK_GDB_server_a01928.srec

 Size     : 61.74 KB 

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 15]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:01.536

Verifying ...

Download verified successfully 

Target is not responding, retrying...

Target is not responding, retrying...

Shutting down...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

This topic has been closed for replies.

5 replies

MM..1
Super User
Jan 29, 2023 10:18 AM UTC

And ? If your code set STOP mode on start ...

DS.4
DS.4Author
Senior
Jan 29, 2023 10:26 AM UTC

 // APPD_Init();

what is this code? it causes it

DS.4
DS.4Author
Senior
Jan 29, 2023 10:36 AM UTC

Ok , better not be running the FUS I guess..

MM..1
Super User
Jan 29, 2023 12:52 PM UTC

You dont ask question , but maybe you try debug ... APPD is aplication daemon ...

On WB firmware save energy is managed with STOP mode then you need setup debuger settings Enable debug in low power modes ENABLED seems enabled then other troubles in your app ( for example power USB overloaded, not preloaded bin firmware usw)

DS.4
DS.4Author
Senior
Jan 29, 2023 1:47 PM UTC

Thanks will try