Skip to main content
nsabo.1
Associate III
Dec 26, 2022 10:59 AM UTC
Question

Graph is not displaying correctly

Receiving data by UART and display it by TOUCHGFX cause some lost data in my screen, graph is not displayed correctly.

There are 2 boards one which is been receiving the signals by sensors and the second one is LCD board which has been configured by TOUCHGFX.

I want to receive data by UART from the first board and show them in LCD.

But some graph is not shown correctly.

Here is the code:

```

HAL_UART_Receive_IT(&huart1,(uint8_t*)RxBuf,20);

HAL_UART_RxCpltCallback(&huart1);

   HAL_Delay(1);

```

I put ```HAL_Delay(1); ``` in order to receive data correctly but it does not make sense.

And the data shown by graph:

```

   if(i<123){

dynamicGraph1.addDataPoint(RxBuf[1]+25);

}else

i=0;

```

Note : in image, the first graph is displaying by UART and as you see suddenly a drop appears... and I don't know how to solve it, and the second graph (from above) is the correct signal.

How can I solve it?

Thanks again.

This topic has been closed for replies.

6 replies

nsabo.1
nsabo.1Author
Associate III
Dec 26, 2022 11:20 AM UTC

@Community member​ 

I got those dropped straight lines . I don't know what the problem is

Karl Yamashita
Super User
Dec 26, 2022 1:25 PM UTC

You need to copy and paste your code exactly how you've written it as i have asked in the other post. I'm not sure why you've started a new post? You've pasted the same question.

Then there is this problem below

HAL_UART_Receive_IT(&huart1,(uint8_t*)RxBuf,20);
 
HAL_UART_RxCpltCallback(&huart1); // This is wrong, you don't make this call, the HAL driver does.
 
 HAL_Delay(1);

And where is this code at? It has to be in some function.

 if(i<123){
 
dynamicGraph1.addDataPoint(RxBuf[1]+25);
 
}else
 
i=0;

what code do you have in HAL_UART_RxCpltCallback?

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{ 
	// show your code 
}

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
nsabo.1
nsabo.1Author
Associate III
Dec 27, 2022 8:34 AM UTC

@Community member​ 

Hi, Karl. sorry for my bad English.

  1. void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
  2. {
  3. // show your code
  4. }

Karl where should I use this function?

you mean I put the add data point in UartCALLBACK?

Karl Yamashita
Super User
Dec 27, 2022 9:07 AM UTC

Maybe my YouTube video will help you understand how to receive UART data

https://youtu.be/bCppZf8FKYg

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
nsabo.1
nsabo.1Author
Associate III
Dec 30, 2022 9:35 AM UTC

Thanks