cancel
Showing results for 
Search instead for 
Did you mean: 

Getting the wrong status value from HAL Libabry

MDeva.1
Associate II

Hello,

I configure the DAC using SPI configuration. I am reading the DAC registers value , when register is read back i got wrong status value from HAL Library why these happened?

for(i=0,j=0,k=0;i<=46;i++,j++,k++)

{

Read( SAW_ADD[i],SAW_Val[j],SAW_RDD[k]);

}

void Read( uint16_t add, uint16_t data,uint16_t Read_add)

{

HAL_GPIO_WritePin(CS_GPIO_Port, CS_Pin, GPIO_PIN_RESET);

status2=HAL_SPI_Transmit(&hspi4, (uint8_t*)&Read_add, sizeof(add),100);

status3=HAL_SPI_Receive(&hspi4, (uint8_t*)&Read_value, sizeof(add),100);

HAL_GPIO_WritePin(CS_GPIO_Port, CS_Pin, GPIO_PIN_SET);

printf("s=%ds=%dAdd=%xValue=%x\n\n\r",status2,status3,Read_add,Read_value);

HAL_Delay(100);

}

0693W00000Y6pvfQAB.png0693W00000Y6pvaQAB.png

2 REPLIES 2
gbm
Principal

To kkep it short: use TransmitReceive / send and receive data at the same time. That's how the SPI works.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Perhaps use local variables rather than globals

Use the sizeof() the variable you're referring too rather than another.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..