Skip to main content
Associate III
Dec 23, 2022 11:08 AM UTC
Question

Waking up Cortex M4 from Cortex A7-0 in STM32MP1 for Bare metal.

we are developing the application by using STM32MP1 processor in bare metal.

we are able to wake up Cortex A7-1 from Cortex A7-0 both are working fine. Now we tried to wake up Cortex M4 from Cortex A7-0,But we are unable to wakeup Cortex M4 from Cortex A7-0.

Individually Cortex M4 is working fine with JTAG .and we can able to wake up Cortex M4 from UBOOT By using RPROC commands .

But in our application we need to wake up Cortex M4 from cortex A7-0 in bare metal. Can you give the sequence of waking up cortex-m4 from Cortex-A7-0 in Bare metal.

So please help us in this.

This topic has been closed for replies.

8 replies

PatrickF
ST Employee
Dec 23, 2022 4:37 PM UTC

Hi,

Maybe share more information than "we are unable to wakeup Cortex M4 from Cortex A7-0" could help.

What did not work ? What did you tried and what are the issue ?

As you are in bare-metal, did you try to debug both A7 and M4 together using JTAG (e.g. using Lauterbach Trace32 tool) ?

Did you check HDP view of internal power control signals to confirm what is going wrong?

Wake-up mechanism depend on which low power mode the Cortex-M4 is:

0693W00000Y6ohmQAB.pngFor Run or Csleep, any NVIC interrupts could be used.

For CStop, which requires EXTI, please refer to RefMan "STM32MP157 EXTI Events".

I think you could use IPCC (EXTI61 or 62), HSEM_IT2 (EXTI64) or Cortex-A SEV (EXTI66) which could be triggered from Cortex-A7 actions and, when set in EXTI, could wakeup Cortex-M4 (and as well trigger NVIC interrupts in Run or CSleep).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Srikanth1Author
Associate III
Dec 29, 2022 5:08 AM UTC

Hi,

Thanks for the reply

We referred 10.3.14 chapter in stm32mp157a processor reference manual for waking up Cortex-M4 in stm32mp157a.

Below are the steps we followed

1.Clearing the MCU_BOOT bit in RCC Global control Register(0x5000010C)

2.Making MCU_RST low in RCC Global Reset control Set_Register(Address:0x50000404)

3.We are coping Cortex-M4 bin file in RETRAM(Address:0x38000000).

4.We are setting Coprocessor state(C_RUN) in TAMP Backup Register(0x5C00A148).

6.We are setting Coprocessor Resource Table address as 0 in TAMP Backup Register(0x5C00A144).

Is it Correct way to wakeup cortex-M4 from Coretx-A7 in stm32mp157a processor?

If not ,we want actual procedure for waking up cortex-M4 from Cortex-A7 in stm2mp157a processor.

regards

srikanth

PatrickF
ST Employee
Jan 3, 2023 9:47 AM UTC

Hi @Srikanth​ 

sequence could be :

  1. RCC_MP_GCR.BOOT_MCU = 0 (should be the case by default after a system reset)
  2. RCC_MP_GRSTCSETR.MCURST = 1 (not needed after a system reset)
  3. Load Cortex-M4 binary in RETRAM and in SRAMx if needed (ensure correct value for initial SP and reset vector, which should be an odd value by definition for Cortex-M4). Refer also to PM0214
  4. RCC_MP_GCR.BOOT_MCU = 1

No need to play with backup registers as you are in bare-metal.

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Srikanth1Author
Associate III
Jan 12, 2023 11:28 AM UTC

Hi,

Thanks for the reply.

We followed

  1. RCC_MP_GCR.BOOT_MCU = 0 (should be the case by default after a system reset)
  2. RCC_MP_GRSTCSETR.MCURST = 1 (not needed after a system reset)
  3. Load Cortex-M4 binary in RETRAM(we kept the cortex M4 binary in RETRAM).
  4. RCC_MP_GCR.BOOT_MCU = 1

But M4 code is not running.

Is there any steps need to take care of M4 code?

Is there any other procedure for waking up M4 from A7?

PatrickF
ST Employee
Jan 13, 2023 8:24 AM UTC

This should be ok.

Once started, did you success to debug your M4 code with JTAG to see what is going wrong ? Maybe a missing init on some clocks or resources used by your code.

If RETRAM is declared as cacheable form A7 side, you should manage the data cache to be sure data are effectively written in the RETRAM memory.

Note that loading Cortex-M4 in RETRAM from A7 should be done from address 0x38000000 onward, whereas the Cortex-M4 code should be compiled with vector table in 0 and code execution in the RETRAM range 0 to 0xFFFF.

Btw, did you check that you have right SP initial value and Reset vector (must be an odd value) at respectively address 0x38000000 and 0x38000004 (or 0 and 4 seen by Cortex-M4)?

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PatrickF
ST Employee
Jan 3, 2023 4:38 PM UTC
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent