Skip to main content
Javier1
Principal
December 1, 2022
Solved

OH boy... I bricked my nucleo Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF

  • December 1, 2022
  • 17 replies
  • 6461 views

I was happily debugging some code in my NUCLEO-F207ZG, the whole morning the debug sessions (stm32cubeIDE) have been quite glitchy.

Until the mcu somehow got briked and i cannot revive it.

I suspect noise in the SW lines comming from some external LEDs nearby had something to do with this issue, or power fluctuations when programming.

I am unable to Read the FLash content so i connected the board to the stCUBEProgrammer.

12:42:36:814 : STLinkUSBDriver.dll loaded
 12:42:36:819 : STLinkUSBDriver.dll loaded
 12:42:36:819 : ST-LINK SN : 066FFF323239524257191044
 12:42:36:820 : ST-LINK FW : V2J39M27
 12:42:36:821 : Board : NUCLEO-F207ZG
 12:42:36:821 : Voltage : 3.24V
 12:42:36:836 : SWD freq : 4000 KHz
 12:42:36:837 : Connect mode: Under Reset
 12:42:36:837 : Reset mode : Hardware reset
 12:42:36:838 : Device ID : 0x411
 12:42:36:850 : Revision ID : Rev 2.0
 12:42:36:871 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x411.stldr is loaded
 12:42:36:871 : STLinkUSBDriver.dll loaded
 12:42:36:871 : ST-LINK SN : 066FFF323239524257191044
 12:42:36:872 : ST-LINK FW : V2J39M27
 12:42:36:872 : Board : NUCLEO-F207ZG
 12:42:36:882 : Voltage : 3.24V
 12:42:36:892 : SWD freq : 4000 KHz
 12:42:36:892 : Connect mode: Under Reset
 12:42:36:892 : Reset mode : Hardware reset
 12:42:36:906 : Device ID : 0x411
 12:42:36:910 : Revision ID : Rev 2.0
 12:42:36:910 : Debug in Low Power mode is not supported for this device.
 12:42:36:910 : Reading data...
 12:42:36:910 : r ap 0 @0x1FFF7A22 0x00000004 bytes Data 0x0000201F
 12:42:36:910 : failed to read the requested memory content
 12:42:37:108 : UPLOADING OPTION BYTES DATA ...
 12:42:37:109 : Bank : 0x00
 12:42:37:109 : Address : 0x40023c14
 12:42:37:109 : Size : 12 Bytes
 12:42:37:109 : Reading data...
 12:42:37:109 : r ap 0 @0x40023C14 0x0000000C bytes Data 0x0FFFFFED
 12:42:37:110 : UPLOADING OPTION BYTES DATA ...
 12:42:37:110 : Bank : 0x00
 12:42:37:110 : Address : 0x40023c14
 12:42:37:110 : Size : 12 Bytes
 12:42:37:110 : Reading data...
 12:42:37:110 : r ap 0 @0x40023C14 0x0000000C bytes Data 0x0FFFFFED
 12:42:37:111 : UPLOADING ...
 12:42:37:111 : Size : 1024 Bytes
 12:42:37:111 : Address : 0x8000000
 12:42:37:111 : Read progress:
 12:42:37:111 : Reading data...
 12:42:37:111 : r ap 0 @0x08000000 0x00000400 bytes Data 0x201F6411
 12:42:37:111 : Error: Data read failed

What ****** me off is the OB->RDP suddenly shows as FF (read protection), im unable to change it back to AA (no read protection).

12:42:58:775 : UPLOADING OPTION BYTES DATA ...
 12:42:58:775 : Bank : 0x00
 12:42:58:775 : Address : 0x40023c14
 12:42:58:775 : Size : 12 Bytes
 12:42:58:776 : Reading data...
 12:42:58:776 : r ap 0 @0x40023C14 0x0000000C bytes Data 0x0FFFFFED
 12:43:02:844 : Option byte command : -ob RDP=170 
 12:43:02:847 : PROGRAMMING OPTION BYTES AREA ...
 12:43:02:848 : Bank : 0x00
 12:43:02:849 : Address : 0x40023c14
 12:43:02:849 : Size : 12 Bytes
 12:43:02:849 : OB buffer: edaaff0fc000001300000000
 12:43:02:849 : Buffer program...
 12:43:02:854 : halt ap 0 
 12:43:02:854 : w ap 0 reg 15 PC (0x20000000) 
 12:43:02:855 : w ap 0 reg 17 MSP (0x20000500) 
 12:43:02:856 : w ap 0 reg 16 xPSR (0x01000000) 
 12:43:02:858 : w ap 0 @0x20000D80 0x00000200 bytes Data 0x00000000
 12:43:02:858 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
 12:43:02:877 : w ap 0 @0x20000004 0x00000940 bytes Data 0xF000B580
 12:43:02:877 : w ap 0 @0x20000D80 0x0000000C bytes Data 0x0FFFAAED
 12:43:02:877 : Loader write option bytes...
 12:43:02:877 : Init flashloader...
 12:43:02:877 : halt ap 0 
 12:43:02:878 : w ap 0 reg 0 R0 0x00000001
 12:43:02:878 : w ap 0 reg 1 R1 0x00000000
 12:43:02:878 : w ap 0 reg 2 R2 0x00000000
 12:43:02:878 : w ap 0 reg 3 R3 0x00000000
 12:43:02:878 : w ap 0 reg 4 R4 0x00000000
 12:43:02:878 : w ap 0 reg 5 R5 0x00000000
 12:43:02:880 : w ap 0 reg 6 R6 0x00000000
 12:43:02:881 : w ap 0 reg 7 R7 0x00000000
 12:43:02:883 : w ap 0 reg 8 R8 0x00000000
 12:43:02:884 : w ap 0 reg 9 R9 0x00000000
 12:43:02:884 : w ap 0 reg 10 R10 0x00000000
 12:43:02:885 : w ap 0 reg 11 R11 0x00000000
 12:43:02:885 : w ap 0 reg 12 R12 0x00000000
 12:43:02:888 : w ap 0 reg 13 SP 0x00000000
 12:43:02:888 : w ap 0 reg 14 LR 0x20000001
 12:43:02:889 : w ap 0 reg 15 PC 0x20000005
 12:43:02:889 : w ap 0 reg 16 xPSR 0x01000000
 12:43:02:890 : w ap 0 reg 17 MSP 0x20000D40
 12:43:02:890 : w ap 0 reg 18 PSP 0x00000000
 12:43:02:891 : run ap 0 
 12:43:02:894 : halt ap 0 
 12:43:02:895 : r ap 0 reg 0 R0 0x00000001
 12:43:02:896 : w ap 0 reg 0 R0 0x40023C14
 12:43:02:897 : w ap 0 reg 1 R1 0x0000000C
 12:43:02:900 : w ap 0 reg 2 R2 0x20000D80
 12:43:02:900 : w ap 0 reg 3 R3 0x00000002
 12:43:02:901 : w ap 0 reg 4 R4 0x00000000
 12:43:02:902 : w ap 0 reg 5 R5 0x00000000
 12:43:02:904 : w ap 0 reg 6 R6 0x00000000
 12:43:02:906 : w ap 0 reg 7 R7 0x00000000
 12:43:02:907 : w ap 0 reg 8 R8 0x00000000
 12:43:02:912 : w ap 0 reg 9 R9 0x00000000
 12:43:02:913 : w ap 0 reg 10 R10 0x00000000
 12:43:02:914 : w ap 0 reg 11 R11 0x00000000
 12:43:02:914 : w ap 0 reg 12 R12 0x00000000
 12:43:02:914 : w ap 0 reg 13 SP 0x00000000
 12:43:02:915 : w ap 0 reg 14 LR 0x20000001
 12:43:02:916 : w ap 0 reg 15 PC 0x200000DF
 12:43:02:917 : w ap 0 reg 16 xPSR 0x01000000
 12:43:02:917 : w ap 0 reg 17 MSP 0x20000D40
 12:43:02:918 : w ap 0 reg 18 PSP 0x00000000
 12:43:02:918 : run ap 0 
 12:43:06:294 : UPLOADING OPTION BYTES DATA ...
 12:43:06:295 : Bank : 0x00
 12:43:06:295 : Address : 0x40023c14
 12:43:06:295 : Size : 12 Bytes
 12:43:06:295 : Reading data...
 12:43:06:297 : r ap 0 @0x40023C14 0x0000000C bytes Data 0x0FFFFFED
 12:43:06:297 : OPTION BYTE PROGRAMMING VERIFICATION:
 12:43:06:297 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
 12:43:06:317 : Error: Option Byte Programming failed
 12:43:06:348 : Time elapsed during option Bytes configuration: 00:00:03.449
 12:43:06:412 : UPLOADING OPTION BYTES DATA ...
 12:43:06:412 : Bank : 0x00
 12:43:06:412 : Address : 0x40023c14
 12:43:06:412 : Size : 12 Bytes
 12:43:06:413 : Reading data...
 12:43:06:413 : r ap 0 @0x40023C14 0x0000000C bytes Data 0x0FFFFFED

Maybe i killed the flash somehow?

I tested with different nucleo boards and everything seems alright with CUBEProgrammer and CUBEide

This topic has been closed for replies.
Best answer by Tesla DeLorean

If you use debug functionality, I think Cube Programmer has this, you should be able to see it with the PC in the 0x1FFF0000 type address range.

>>I am going to explore this, it could be caused by a broken mcu?

I suppose, but several aspects seem to be otherwise functional. You might want to submit this as an Online Support Request thing, see if the FAE have any insight or info off the large issue FAQ they consult.

17 replies

Javier1
Javier1Author
Principal
December 1, 2022

This topic has been around the forum in the past so i assume there is many different ways to end up in this situation.

  •  here, @Piranha​ suggests to update the stlink firmware and perform a mass erase operation.

Which for me ends up showing

Error: Mass erase operation failed.Please verify flash protection
  • here, @VVakh.1​ tries to set the OB->RCP bytes to AA, with the same luck i have.
Error: Option Byte Programming failed

  •  
hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

I bricked another nucleo-f207zg board.

this time i can read but i cannot write flash

16:43:03:005 : Error: Uploading Option Bytes bank: 0 failed
 16:43:03:034 : Error: Reloading Option Bytes Data failed

OB->RDP=0xFF as before and i cannot change it

edit: when i unplugged and plugged it again now it fails the exact same way as the previous nucleo.

Now i have two identicaly bricked nucleo boards.

16:49:38:271 : Error: Expected value for Option Byte "RDP": 0xAA, found: 0xFF
 16:49:38:300 : Error: Option Byte Programming failed

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

Lets try out this ST video

https://www.youtube.com/watch?v=f7vs0NwZPFo

Edit: that was not very helpful

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

Reading the PM0075 Reading/programming the embedded Flash memory APP note now

https://www.st.com/resource/en/programming_manual/pm0075-stm32f10xxx-flash-memory-microcontrollers-stmicroelectronics.pdf

0693W00000WK0YzQAL.png 

it says the unprotect value should be A5 but the cubePRogrammer is trying to write AA..... maybe thats the key to unlock the mcu?

0693W00000WK0aCQAT.png 

im going o try to set the OB-RDP bytes with STM32_Programmer_CLI.exe

https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#

for me is located (default windows instalation) under

cd \Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin

comprehensive tutorial https://blog.katastros.com/a?ID=01800-259412d1-e075-427a-b4d9-912db0f0f5c6

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

Connecting via SWD

STM32_Programmer_CLI.exe -c port=SWD

 0693W00000WK0oiQAD.png

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

Writting into the OB bytes

STM32_Programmer_CLI.exe -c port=SWD freq=4000 -e 0 -w32 0x40023C14 0x0FFFA5ED

0693W00000WK0szQAD.png 

NAh it didnt work....

hit me up in https://www.linkedin.com/in/javiermuñoz/
Javier1
Javier1Author
Principal
December 1, 2022

This guy had the same problem as i am having right now

https://www.eevblog.com/forum/microcontrollers/stm32-dead-flash/

Describes perfectly what happened to me 4 hours ago, no solution was shared

hit me up in https://www.linkedin.com/in/javiermuñoz/
Tesla DeLorean
Guru
December 1, 2022

What's your code doing to get the boards/chips in this state?

Does behaviour change if BOOT0 is strapped to VDD? There's a jumperable spot on the side of CN11

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Javier1
Javier1Author
Principal
December 2, 2022

Thanks @Community member​ ..

>>What's your code doing to get the boards/chips in this state?

In dont think code its the issue here, there is some DMA activity with the ADCs but 1ms spaced.

The boards get in this state when i connect them to a test rig im developing for other boards.

I suspect the test rig is killing the nucleos.

>>Does behaviour change if BOOT0 is strapped to VDD? There's a jumperable spot on the side of CN11

Going to try this

0693W00000WK4VBQA1.png 

Edit: I soldered a wire from BOOT0 to 3v3, then i connected the USB, i get the same results as before.

How do i know the mcu is in ROM system bootloader? i connected an USB cable to the USB OTG port and cubeProgrammer couldnt detect any DFU port.

hit me up in https://www.linkedin.com/in/javiermuñoz/
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
December 2, 2022

If you use debug functionality, I think Cube Programmer has this, you should be able to see it with the PC in the 0x1FFF0000 type address range.

>>I am going to explore this, it could be caused by a broken mcu?

I suppose, but several aspects seem to be otherwise functional. You might want to submit this as an Online Support Request thing, see if the FAE have any insight or info off the large issue FAQ they consult.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Visitor II
May 25, 2024

Did you find anything out about this issue? I'm having the exact same issue with my stm32F401

Visitor II
March 12, 2025

If you open st-link utility you will find more settings than are in the cube programmer. I had similar problem in my case it was PCROP_RDP checkbox in the Option Byte window. I have unchecked it and my stm32 device started to function normally. At least you may experiment with other additional settings which cube programmer lack by unknown reason...