Skip to main content
HHuyn.15
Associate II
Nov 30, 2022 1:04 AM UTC
Solved

Did CubeMX 6.7 break H7 Clock Configuration?

Hi,

I have just updated to CubeMx 6.7 and now my stm32H755 nucleo board shows error while setting to 480MHz. I'm pretty sure that this board can run this fast before.

Did the new CubeMx break clock config feature for H7 devices?

0693W00000WJnaxQAD.png 

There is also this crazy aliasing issue with the UI refresh while I move the mouse to select the option. Does anyone know how to get rid of this?

0693W00000WJnbgQAD.png 

Thank you.

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Dec 1, 2022 11:30 PM UTC

To get 480 MHz, go to the RCC parameters and check that the product revision is "V".

For some reason the default is "Y".

Then set the power regulator voltage scale to 0.

​

4 replies

Foued_KH
ST Employee
Dec 1, 2022 10:23 PM UTC

Hello @Community member​,

Thanks for bringing this issue to our attention. I reported it to our STM32CubeMX team.

Internal ticket number: 140578 (This is an internal tracking number and is not accessible or usable by customers).

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Pavel A.
Pavel A.Best answer
Dec 1, 2022 11:30 PM UTC

To get 480 MHz, go to the RCC parameters and check that the product revision is "V".

For some reason the default is "Y".

Then set the power regulator voltage scale to 0.

​

HHuyn.15
HHuyn.15Author
Associate II
Dec 2, 2022 1:36 AM UTC

@Pavel A.​ Awesome! That tweak did the trick for the clock. Thank you.

Visitor II
May 18, 2024 2:36 AM UTC

Thanks for the heads up on the RCC setting bug!

Nucleo-H753ZIT_RCC_Setting_Bug.bmp