VL6180X -- How to achieve a 100 Hz sample rate?
I have a VL6180X that I am running in continuous measurement mode and read from when a hardware interrupt is triggered by the senor. My issue is that I cannot get the sensor to signal at a rate of 100 Hz. Currently, the best I can achieve is 50 Hz.
Has anyone had success with this?
I have read that tweaking the inter-measurement and max convergence times can help, but I am not sure where to start with those values. Any advice would be greatly appreciated :)
Also, within the VL6 API, I noticed that the `VL6180x_RangeSetInterMeasPeriod()` function has the following code block:
/* doc in not 100% clear and confusing about the limit practically all value are OK but 0
* that can hang device in continuous mode */
if (InterMeasTime_msec < 10) {
InterMeasTime_msec = 10;
}This block appears to hard limit the inter-measurement time. Commenting out this check and setting `InterMeasTime_msec=0` helps with reaching 100 Hz, but makes the sensor prone to crashing. Does anyone know why this check exists?