Skip to main content
DPeki.1
Associate II
November 2, 2022
Solved

Should code that runs on F303re Nucleo run on F303ze nucleo? Virtual Comm port issues

Hello. I have a project that runs fine on F303RE Nucleo board. I loaded it on the F303ZE Nucleo board and I get no banner displayed on the Virtual Comm port. The device manager sees the port fine.

Are there any solder bridges or jumpers needed on the ZE board to enable the VCP?

Thanks,

  • Dave
This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
November 3, 2022

You should also note that both NUCLEO use different target packages:

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

KDJEM.1
ST Technical Moderator
November 3, 2022

Hello @DPeki.1​,

Try to connect using STM32Cubeprogrammer.

You can check the solder bridges and jumpers needed on the nucleo-F303ZE board in the UM1974.

Thank you for your contribution.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
November 3, 2022

You should also note that both NUCLEO use different target packages:

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DPeki.1
DPeki.1Author
Associate II
November 3, 2022

Thank you. That explains it. I was naive to think it was just pin configurations differences between the two boards F303RE and F303ZE.

  • Dave