Skip to main content
Gencay
Associate III
August 16, 2022
Solved

I was following this how to create your own machine tutorial and got this warning and my flash_layout directory is empty.

Link to the tutorial and warning:

WARNING: st-image-weston-1.0-r0 do_st_write_license_create_summary: IMG LIC SUM: File does not exist with open file /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp1-test/tmp-glibc/deploy/licenses/st-image-resize-initrd-openstlinux-weston-stm32mp1-test-20220815132043/package.manifest
 

This topic has been closed for replies.

5 replies

Kevin HUBER
ST Employee
August 16, 2022

Hello @Gencay​ ,

I already saw this kind of error, but I can't find again what was the issue. My best lead is when you used the command

DISTRO=openstlinux-weston MACHINE=<machine> source layers/meta-st/scripts/envsetup.sh

A license agreement opens. Did you agree with the license agreement?

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Gencay
GencayAuthor
Associate III
August 16, 2022

Yes I agreed first time when it is asked, I just tried again sourcing the environment but agreement did not come up, below output is displayed:

Linux Distrib: Ubuntu
Linux Release: 20.04
 
Required packages for Linux Distrib:
bsdmainutils build-essential chrpath cpio debianutils diffstat gawk gcc-multilib git iputils-ping libegl1-mesa libgmp-dev libmpc-dev libsdl1.2-dev libssl-dev lz4 pylint python3 python3-git python3-jinja2 python3-pexpect python3-pip socat texinfo unzip wget xterm xz-utils zstd
 
Check OK: all required packages are installed on host.
 
[source layers/openembedded-core/oe-init-build-env][with previous config]
 
===========================================================================
Configuration files have been created for the following configuration:
 
 DISTRO : openstlinux-weston
 DISTRO_CODENAME : kirkstone
 MACHINE : stm32mp1-test
 BB_NUMBER_THREADS : <no-custom-config-set>
 PARALLEL_MAKE : <no-custom-config-set>
 
 BUILDDIR : build-openstlinuxweston-stm32mp1-test
 DOWNLOAD_DIR : /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/Shared/downloads
 SSTATE_DIR : /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/Shared/sstate-cache
 
 SOURCE_MIRROR_URL : <no-custom-config-set>
 SSTATE_MIRRORS : <disable>
 
 WITH_EULA_ACCEPTED: YES
 
===========================================================================
 
Available images for OpenSTLinux layers are:
 
 - Official OpenSTLinux images:
 st-image-weston - OpenSTLinux weston image with basic Wayland support (if enable in distro)
 
 - Other OpenSTLinux images:
 - Supported images:
 st-image-core - OpenSTLinux core image
 
 
You can now run 'bitbake <image>'
 

SMich.1
Senior
August 23, 2022

I have the same issue with the new distro Kirkstone.

My layers working perfect with dunfell.

I made changes for the kirkstine distro and all compiles and i have all the images files but no flashlayouts. :face_with_steam_from_nose:

SMich.1
SMich.1Best answer
Senior
August 23, 2022
Gencay
GencayAuthor
Associate III
August 24, 2022

Thank you so much I will try this one.