FWege.1Associate IIForum|Forum|4 years agoJuly 20, 2022QuestionSTM32CubeProgrammer STM32G474 option bytesForum|Forum|4 years agoJuly 20, 20221 reply1252 viewsDear allI think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.Thanks in advance,FranzSTM32CubeProgrammerBug-reportSTM32G4 series