Skip to main content
Rio1
Visitor II
Jul 5, 2022 6:24 AM UTC
Question

Is STM DCMI driver support Raw Bayer Image format?

I'm interfacing 10-bit camera on DCMI protocol. I can able to read the data over DCMI and display it on the STM32F7508 Discovery board. Since the color format is different I'm not getting the actual real-time colors. I'm using the "Camera" example on STMCUbe IDE. There is no Macro expansion for RAW Bayer. I referred AN502, section 3.6. It says it also supports the Bayer format. Can somebody help me to figure this out? or else do I need to implement demosaicing algorithm?

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Jul 5, 2022 2:20 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Technical Moderator
Jul 20, 2022 9:14 AM UTC

Hi @Rio1​ ,

A similar question is already asked here.

You are right the DCMI support the Raw Bayer format but the DMA2D can't support this format type. You can find the support color mode input for the DMA2D in the RM0385 Table 35.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.