Skip to main content
CMehr.1
Associate
June 10, 2022
Solved

LSM6DSM Power Draw at Different Voltages

  • June 10, 2022
  • 1 reply
  • 1109 views

Hello,

I am looking at the LSM6DSM datasheet for power draws. Here is an example

  • Accelerometer Current Consumption @ ODR=52Hz
    • VDD = 1.8 V
    • Current = 25 uA
    • Power = VDD*Current = 45 uW

Does the current required by the LSM6DSM accelerometer change if VDD is toward the upper end, say, 3.3 V? Should I expect lower, or higher, power draws? Basically fill out the following:

  • Accelerometer Current Consumption @ ODR=52Hz
    • VDD = 3.3 V
    • Current = TBD uA
    • Power = VDD*Current = TBD uW

Thanks in advance!

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @CMehr.1​ ,

    please consider that the main increase in power consumption is given by a change in the ODR frequency.

    A change in Vdd from 1.8V to 3.3V qill increase the accelerometer power consumption by about 2 / 3 uA.

    • VDD = 3.3 V
    • Current = 27uA uA
    • Power = VDD*Current = 90 uW

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    June 17, 2022

    Hi @CMehr.1​ ,

    please consider that the main increase in power consumption is given by a change in the ODR frequency.

    A change in Vdd from 1.8V to 3.3V qill increase the accelerometer power consumption by about 2 / 3 uA.

    • VDD = 3.3 V
    • Current = 27uA uA
    • Power = VDD*Current = 90 uW

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster. 

    -Eleon