Skip to main content
AElta.1
Associate II
May 30, 2022
Question

real time processing in STM32H750B-DK board ?

  • May 30, 2022
  • 0 replies
  • 698 views

I am working on reading an External 3 bit parallel CMOS ADC (4-8 MSPS)(from MAX2771 board or Eva KIT) GNSS digital output through STM32H750B-DK board, Then transmit it over Ethernet or USB2.0 in real time through TCP/IP protocol continuously.

then process the data in MATLAB by reading from the TCP/IP protocol?

I never used STM32 before so I am just wondering if this would work ?

thanks in advance

This topic has been closed for replies.