Skip to main content
JKut
Associate
May 28, 2022 12:13 PM UTC
Question

Post-generation hook in STM32CubeIDE

In our workflow around the code generation and building firmware using STM32CubeIDE, we have certain manual steps after code generation.

Is there a place to hook in a script to be run after code generation completes? Similar to the "Build Steps" which can be configured in Eclipse CDT projects?

This topic has been closed for replies.

6 replies

Pavel A.
May 28, 2022 2:08 PM UTC

Just use the Pre-build step?

JKut
JKutAuthor
Associate
May 28, 2022 4:44 PM UTC

Yeah I'm aware of that option, but "just" using it isn't that simple. Code generation happens in the order of "once in a while", while building is done in the order of "always".

Our post-generation steps are rather lengthy, and also can't be repeated. E.g. applying patches shouldn't be repeated.

Pavel A.
May 28, 2022 4:55 PM UTC

In the script, check if the post-generation is already done, then skip the lengthy things.

JKut
JKutAuthor
Associate
May 28, 2022 5:03 PM UTC

So how do you suppose to do that in a general case, if you don't know nothing about whether and when code generation has happened or not? By the timestamp of a known generated file? Is there a specific candidate file you would have in mind?