Skip to main content
Associate III
May 11, 2022
Solved

How to enable ADC1 on NUCLEO-U575ZI-Q?

I work with STM32CubeIDE 1.9.0, STM32CubeMX 6.5.0, and STM32Cube FW_U5 V1.1.0, on a NUCLEO-U575ZI-Q.

I created a new project for this specific board, and left everything by default.

I need to use the ADC1, wich is enabled by default.

I start with this call:

HAL_ADC_Start(&hadc1);

And it never succeed. Digging deeper, there seem to be a timeout on the ADC1 activation. The register bit ADC_CR_ADEN is set but the corresponding flag ADC_FLAG_RDY never rise.

For information, the ADC voltage regulator was successfuly enabled during system initialization (ADVREGEN set to 1, wait for a time, then check that the corresponding flag is risen). Before rising ADC_CR_ADEN, all bits of the register ADC CR is are low (except ADVREGEN = 1). According to the RM for STM32U575, this is the only condition before enabling the ADC.

Did I miss something in the reference manual, or in the code? Is there something wrong with my STM32U575 chip?

This topic has been closed for replies.
Bastien LSBest answer
Associate III
May 12, 2022

This line was missing:

HAL_PWREx_EnableVddA();

7 replies

Mike_ST
ST Technical Moderator
May 11, 2022

Hello,

Please share your .ioc file and code, if you wish.

Maybe somebody will be able to help.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Mike_ST
ST Technical Moderator
May 11, 2022

By the way, in the STM32Cube FW_U5 V1.1.0 package you have some ADC examples under

Projects\NUCLEO-U575ZI-Q\Examples\ADC\

So you can check what is different with your code.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Associate III
May 11, 2022

Thank you, I will have a look at it.

Bastien LSAuthorBest answer
Associate III
May 12, 2022

This line was missing:

HAL_PWREx_EnableVddA();

meghasb
Associate III
January 4, 2023
  1. @Bastien LS​ hi, did u get the ans for this? even i'm facing the same problem, even after enabling HAL_PWREx_EnableVddA();

is also not working..

can any one help with this?

JCout.11
Visitor II
February 7, 2023

HAL_PWREx_EnableVddA(); placed between MX_ADC1_Init and HAL_ADC_Start in main.c seems to work.

Associate III
August 2, 2024

I have placed the  HAL_PWREx_EnableVddA(); after MA_ADC1_Init() in main.c, still my ADC value is not good. I am getting ADC value as 11 or 12.