Skip to main content
Gpeti
Senior
April 20, 2022
Solved

AES Key management in STM32H7

  • April 20, 2022
  • 3 replies
  • 2719 views

Following this question, I am also confused about how to fill the key in the CRYP peripheral. I don't find the Ref Manual very clear

The register description mentions the key as an array K and an array b where MSB of K are in lowest address register.

But it seems to be different in the key registers section of the doc.

Basically an AES key would be an array of bytes, and I can't figure out how I fill these bytes in the key registers...

0693W00000LySTUQA3.png 

0693W00000LySQGQA3.png

This topic has been closed for replies.
Best answer by Jocelyn RICARD

Hello @Gpeti​ ,

I would guess this is same issue as for IV.

The STM32H7 Cube provides an mbedTLS wrapping to the CRYP peripheral in

STM32Cube_FW_H7_V1.10.0\Projects\STM32H743I-EVAL\Applications\mbedTLS\Crypto_Selftest

You can see in aes_alt.c how the mbedTLS input key is transformed into Cryp compatible key using:

  /* Format and fill AES key */

  for( i=0; i < (keybits/32); i++)

    GET_UINT32_BE( ctx->aes_key[i], key,4*i );

Where GET_UINT32_BE is implemented as:

#define GET_UINT32_BE(n,b,i)              \

{                            \

  (n) = ( (uint32_t) (b)[(i)  ] << 24 )       \

    | ( (uint32_t) (b)[(i) + 1] << 16 )       \

    | ( (uint32_t) (b)[(i) + 2] << 8 )       \

    | ( (uint32_t) (b)[(i) + 3]    );      \

}

This should help you finding the good implementation

Best regards

Jocelyn

3 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
April 20, 2022

Hello @Gpeti​ ,

I would guess this is same issue as for IV.

The STM32H7 Cube provides an mbedTLS wrapping to the CRYP peripheral in

STM32Cube_FW_H7_V1.10.0\Projects\STM32H743I-EVAL\Applications\mbedTLS\Crypto_Selftest

You can see in aes_alt.c how the mbedTLS input key is transformed into Cryp compatible key using:

  /* Format and fill AES key */

  for( i=0; i < (keybits/32); i++)

    GET_UINT32_BE( ctx->aes_key[i], key,4*i );

Where GET_UINT32_BE is implemented as:

#define GET_UINT32_BE(n,b,i)              \

{                            \

  (n) = ( (uint32_t) (b)[(i)  ] << 24 )       \

    | ( (uint32_t) (b)[(i) + 1] << 16 )       \

    | ( (uint32_t) (b)[(i) + 2] << 8 )       \

    | ( (uint32_t) (b)[(i) + 3]    );      \

}

This should help you finding the good implementation

Best regards

Jocelyn

Gpeti
GpetiAuthor
Senior
April 21, 2022

Perfect ! I had a look to the AES example project but not in mbedTLS.

thank you

Gpeti
GpetiAuthor
Senior
April 22, 2022

Hello, I had a closer look to the GitHub example code, and it's still confusing. the example you copied tends to indicate that the Key and IV registers are big-endian (GET_UINT32_B converts an array of 4 bytes into a big-endian represented 32 bits value). However the ref manual says:

The swapping operation concerns only the CRYP_DOUT and CRYP_DIN registers. The

CRYP_KxL/KxR and CRYP_IVxL/IVxR registers are not sensitive to the swap mode

selected.They have a fixed little-endian configuration