Solved
Is it possible to use a timer to send a on-time-pulse PWM at a frequency of less than 1Hz?
For example, sending a 1.5second on-time pulse? It would also be helpful to be able to set a delay before the pulse starts as well as the 'repetition' of the pulse. The TIMER1 does have the required features but not sure how to scale down the frequency to under 1Hz. Should I chain timers as master/slave to obtain the low frequency?
Thanks!