Can anyone explain how to enable the ADC Clock Source on an STM32H753ZI using STM32 Cube?
- 15 replies
- 10315 views
I'm new to Cube IDE and Cube MX but I've been trying to create a simple project based on an STM32H753ZI to investigate ADC capture.
Having enabled a few channels on ADC3 I looked in the clock tree to find the ADC clock speed but it's greyed out. When I hover over the ADC Clock Mux section I get a message saying "ADC Clock Source is not available" and to configure one in the Pinout Tab ADC.
I can't see any options that mention anything to do with a clock in the ADC section (or , I've seen screenshots from the STM32H743 where there is a "Clock Prescaler" option under ADC_Settings, but I don't see this option in my case. I've seen that sometimes options only become visible when other options have first been set, so hopefully this is something simple that I've overlooked.
Any help would be welcomed.