Skip to main content
VLacr.1
Associate II
Jan 14, 2022 9:27 AM UTC
Question

How to connect STM32H745I-DISCO with openOCD using openOCD ?

Hello,

I am not able to connect my ubuntu 20.04 laptop to a STM32H745I-DISCO board using openocd.

```

$ openocd -f board/stm32h745i-disco.cfg

Open On-Chip Debugger 0.11.0+dev-00450-ge67ff42de (2022-01-14-09:58)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

Error: The specified debug interface was not found (hla)

The following debug adapters are available:

1: jlink

2: buspirate

```

I tried with the following revisions of openocd:

  • revision 0.11 from official repository
  • master version from ST Fork

I see the interface on my computer:

```

$ lsusb | grep -i stm

Bus 001 Device 016: ID 0483:374e STMicroelectronics STLINK-V3

```

Did I missed something ?

This topic has been closed for replies.

3 replies

Andreas Bolsch
Lead III
Jan 14, 2022 7:08 PM UTC

Looks like you've build both variants by yourself? Then most probably the hla interface wasn't built in (maybe some dependency was missing so that 'configure' script did exclude it automatically --- check configure's output).

vlacr.11
Associate II
Jan 17, 2022 10:40 AM UTC

Thanks for your answer Andreas. I tried to compile with:

```

./configure --enable-stlink

```

The ST Fork of openOCD doesn't compile:

```

./src/helper/types.h:194:9: error: ‘misc_items’ may be used uninitialized in this function [-Werror=maybe-uninitialized]

 194 | buf[0] = (uint8_t) (val >> 0);

     | ~~~~~~~^~~~~~~~~~~~~~~~~~~~~~

src/jtag/drivers/stlink_usb.c:4595:20: note: ‘misc_items’ was declared here

 4595 | unsigned int cnt, misc_items;

     |                   ^~~~~~~~~~

```

However, the official openOCD compiles with this option.

Going back to the board with this new openocd, it seems that I have at least an access right issue:

```

$ openocd -f board/stm32h745i-disco.cfg

Open On-Chip Debugger 0.11.0-dirty (2022-01-17-09:32)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 1800 kHz

Error: libusb_open() failed with LIBUSB_ERROR_ACCESS

Error: open failed

```

When I try to bypass this issue, I run into another one:

```

$ sudo openocd -f board/stm32h745i-disco.cfg

Open On-Chip Debugger 0.11.0-dirty (2022-01-17-09:32)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 1800 kHz

Info : STLINK V3J3M2 (API v3) VID:PID 0483:374E

Info : Target voltage: 3.279681

Error: init mode failed (unable to connect to the target)

```

Any clue ?

GTelk
Associate II
Oct 19, 2022 8:51 PM UTC

There is an unititialized variable in stlink_usb.c, see https://github.com/STMicroelectronics/OpenOCD/pull/13