Skip to main content
xpress_embedo
Associate III
Jan 8, 2022 7:54 AM UTC
Question

STemWin_HelloWorld Example Debugging and GUI_Delay Not Working

Hello Everyone

I am trying to use STemWin with STM32CubeIDE, but facing a lot of problems.

I have STM32F769I Discovery Board with me, and I have downloaded the CubeF7 package which already has few examples related to STemWin, I took the simple example of HelloWorld available as "STemWin_HelloWorld" in the CubeF7 Package.

It works fine, but I am facing two issues.

  • First When I am debugging using single stepping, I don't see anything on display.
  • Second, I modified the software little bit to display another string on display with some delay and the string after delay which I wanted to display is not displaying on the screen.

The following is the program without delay i.e. GUI_Delay and it works if I program and don't do single step debugging.

void MainTask(void) {
 GUI_Clear();
 GUI_SetFont(&GUI_Font32_1);
 GUI_DispString("Hello World from STM32F7\r\n");
 GUI_DispStringAt("Hello world!", (LCD_GetXSize()-100)/2, (LCD_GetYSize()-20)/2); 
 while(1);
}

But when I updated the above program by adding a simple delay of 1 second, it stops displaying the second Hello World message after GUI_Delay.

void MainTask(void) {
 GUI_Clear();
 GUI_SetFont(&GUI_Font32_1);
 GUI_DispString("Hello World from STM32F7\r\n");
 GUI_Delay(1000);
 GUI_DispStringAt("Hello world!", (LCD_GetXSize()-100)/2, (LCD_GetYSize()-20)/2); 
 while(1);
}

0693W00000HqtA8QAJ.pngAlso GUI_Delay is not blocking I can see my control reaching while(1) as shown in the below image.

0693W00000HqtBGQAZ.png 

Since this is an example project and I am using demo board from ST, my expectation would be that this should work out of the box.

Can someone please support me with this?

This topic has been closed for replies.

2 replies

xpress_embedo
Associate III
Jan 10, 2022 11:58 AM UTC

Hi @Imen DAHMEN​ 

Can you please help here?

I am using CubeF7 MCU package example project (not any custom project), and it is not working as intended.

Can you please support here?

Thanks in advance

ST Technical Moderator
Feb 4, 2022 2:44 PM UTC

Hello @xpress_embedo​ ,

I suggest to keep all comments regarding this issue on this discussion: Help Needed in Building a Simple Project with STemWin and STM32CubeIDE

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks