Skip to main content
MRall.1
Visitor II
December 1, 2021
Solved

How to enable the kernel splashscreen on STM32MP157 board , kernel 5.4 and LCD RGB interface ?

Hi,

I'm using a STM32MP157a with yocto dunfell with 5.4 kernel version, and I'm trying to enable the kernel splashscreen. On my board I'm using the RBG lcd interface, and when the system is UP my application in showing curretly. On kernel config I have enabled the flags:

LOGO

LOGO_LINUX_CLUT224

FRAMEBUFFER_CONSOLE

but no tux are showing at startup...

Where I'm wrong ?

This topic has been closed for replies.
Kevin HUBER
Kevin HUBERBest answer
ST Employee
January 10, 2022

Hi @MRall.1​ ,

To enable the spashscreen when building from Yocto, you have to build these two recipes:

  • layers/meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm
  • layers/openembedded-core/meta/recipes-core/psplash

The file psplash-drm.bb adds the file psplash-drm-start.service to your filesystem.

Once you are on the board, you must have something like that (I am on OpenSTLinux 5.10 so some paths may be different):

root@stm32mp1:/# find -name "psplash*"
./etc/systemd/system/local-fs.target.wants/psplash-drm-start.service
./lib/systemd/system/psplash-drm-start.service
./usr/bin/psplash-drm
./usr/bin/psplash-drm-quit
./var/lib/dpkg/info/psplash-drm.list
./var/lib/dpkg/info/psplash-drm.md5sums
./var/lib/dpkg/info/psplash-drm.postinst
./var/lib/dpkg/info/psplash-drm.prerm

Hope it helps,

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Kevin HUBER
Kevin HUBERBest answer
ST Employee
January 10, 2022

Hi @MRall.1​ ,

To enable the spashscreen when building from Yocto, you have to build these two recipes:

  • layers/meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm
  • layers/openembedded-core/meta/recipes-core/psplash

The file psplash-drm.bb adds the file psplash-drm-start.service to your filesystem.

Once you are on the board, you must have something like that (I am on OpenSTLinux 5.10 so some paths may be different):

root@stm32mp1:/# find -name "psplash*"
./etc/systemd/system/local-fs.target.wants/psplash-drm-start.service
./lib/systemd/system/psplash-drm-start.service
./usr/bin/psplash-drm
./usr/bin/psplash-drm-quit
./var/lib/dpkg/info/psplash-drm.list
./var/lib/dpkg/info/psplash-drm.md5sums
./var/lib/dpkg/info/psplash-drm.postinst
./var/lib/dpkg/info/psplash-drm.prerm

Hope it helps,

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.