Skip to main content
JBond.1
Senior
October 9, 2021
Solved

FR_LOCKED issue when writing to file with FATFS R0.12c over SDIO

  • October 9, 2021
  • 8 replies
  • 3969 views

Hi, I have STM32F407 and trying to write log file (in main loop) with FATFS R0.12c over SDIO.

But after few writes I get error:

FR_LOCKED // (16) The operation is rejected according to the file sharing policy

Previously I was using STM32F103 and was writing to log file using same algorithm with FATFS R0.11 over SPI without this issue. So I suspect the issue should be in "FATFS R0.12c" or "SDIO"?

What could be the issue and how could I fix this?

This topic has been closed for replies.
Best answer by Tesla DeLorean

No they all have their own FIFO.

What however is critical is not to get distracted in the middle of SDIO transfers, the FIFO protects you somewhat, but you can't go off into other interrupts/threads for prolonged periods.

DMA would be preferable.

In polled you might want to look at the SDIO peripheral library, perhaps optimizing the aligned memory case, or using a "critical section"

8 replies

JBond.1
JBond.1Author
Senior
October 9, 2021

It seems that first I am getting

FR_DISK_ERR // (1) A hard error occurred in the low level disk I/O layer

from f_lseek.

And after that it becomes

FR_LOCKED // (16) The operation is rejected according to the file sharing policy

JBond.1
JBond.1Author
Senior
October 9, 2021

Why do I get FR_DISK_ERR on f_lseek?

Tesla DeLorean
Guru
October 9, 2021

Who knows?

Probably has an issue loading and walking the FAT Table.

Instrument the DISKIO layer so you can establish the point of failure and the error the underlying driver code is reporting.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JBond.1
JBond.1Author
Senior
October 10, 2021

OK, with your encouragement I did dig deeper. I set the break point in "bsp_driver_sd.c" where it returns "hsd->ErrorCode" from "HAL_SD_ReadBlocks":

__weak uint8_t BSP_SD_ReadBlocks(uint32_t *pData, uint32_t ReadAddr, uint32_t NumOfBlocks, uint32_t Timeout)
{
 uint8_t sd_state = MSD_OK;
 
 if (HAL_SD_ReadBlocks(&hsd, (uint8_t *)pData, ReadAddr, NumOfBlocks, Timeout) != HAL_OK)
 {
 sd_state = MSD_ERROR; // break point, check hsd->ErrorCode 
 }
 
 return sd_state;
}

Writing to file sometimes works, but eventually it returns "hsd->ErrorCode = 0x20" which means HAL_SD_ERROR_RX_OVERRUN:

#define HAL_SD_ERROR_RX_OVERRUN SDMMC_ERROR_RX_OVERRUN //!< Receive FIFO overrun
#define SDMMC_ERROR_RX_OVERRUN 0x00000020U //!< Receive FIFO overrun

How do I fix HAL_SD_ERROR_RX_OVERRUN?

I dont use DMA, my settings

0693W00000FBzjxQAD.png0693W00000FBzjsQAD.png