Skip to main content
MBolo.1
Associate III
Oct 4, 2021 4:16 AM UTC
Solved

Some help with the USB on the STM32F446VET .

Hi , I'm writing here to ask community some help with the F446VET chip. I tried the Cube Ide and CubeMX to perform all the settings.

What have been done so far :

  1. In the USB_DEVICE--> Class for FS IP is set to "Communication Device Class(Virtual Port Com)"
  2. In the RCC->HSE and LSE are both enabled (pins PH0/PH1 and PC14/PC15)
  3. I use the PA12/PA11 pins as for USB
  4. And in the USB_OTG_FS Mode is set to Device_Only .

After I flash the code generated on the board and connect through the USB connected to the pins A12 and A11 Windows is continuously trying to recognize the device , over and over again with the message "Device Description Failed " . Tried on other laptop and the same stuff.

Other suggestions and help would be appreciated, thank you.

This topic has been closed for replies.
MBolo.1
MBolo.1Best answer
Associate III
Dec 5, 2021 3:55 AM UTC

Hi, to everyone who looked here I eventually found the solution.

In the usbd_cdc_if.c file had to add this code :

1
 /* USER CODE BEGIN INCLUDE */
#define APP_RX_DATA_SIZE 2048// !!! aded by me
#define APP_TX_DATA_SIZE 2048
/* USER CODE END INCLUDE */
 2 
/* Private variables ---------------------------------------------------------*/
uint8_t buffer[7]; //!!!!!!Added by me
/* USER CODE END PV */
 3 
case CDC_SET_LINE_CODING:
 		 buffer[0]=pbuf[0]; //////////Added by me
 			buffer[1]=pbuf[1];
 	 	 	buffer[2]=pbuf[2];
 	 	 	buffer[3]=pbuf[3];
 	 	 	buffer[4]=pbuf[4];
 	 	 	buffer[5]=pbuf[5];
 	 	 	buffer[6]=pbuf[6];
 
 break;
 
 case CDC_GET_LINE_CODING:
 			pbuf[0]=buffer[0];
 	 	 	pbuf[1]=buffer[1];
 	 	 	pbuf[2]=buffer[2];
 	 	 	pbuf[3]=buffer[3];
 	 	 	pbuf[4]=buffer[4];
 	 	 	pbuf[5]=buffer[5];
 	 	 	pbuf[6]=buffer[6];
static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
 /* USER CODE BEGIN 6 */
 USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
 USBD_CDC_ReceivePacket(&hUsbDeviceFS);
 CDC_Transmit_FS(Buf, *Len); // ADED BY ME !!!!!!!!!!!!!
 return (USBD_OK);
 /* USER CODE END 6 */
}

and this solves the problem.

Moderator you can consider this problem closed.

3 replies

Mike_ST
ST Technical Moderator
Oct 4, 2021 1:14 PM UTC

In the F4 software package:

https://www.st.com/en/embedded-software/stm32cubef4.html

(CubeMX automatically donwload it on your PC, default dir is C:\Users\Login\STM32Cube\Repository)

There is an example:

STM32Cube_FW_F4_V1.26.2\Projects\STM32446E_EVAL\Applications\USB_Device\CDC_Standalone

Please compare the 2 projects to find what is missing.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
MBolo.1
MBolo.1Author
Associate III
Oct 5, 2021 4:30 PM UTC

Hi, thank you for your answer. I checked the files how you recommended and everything looks fine.

Today a connected the logical analyzer to the usb connector to see what signals I'm getting and this are the signals

0693W00000FBXOmQAP.jpgthe rest of them a repeating and they are similar to this one.

MBolo.1
MBolo.1AuthorBest answer
Associate III
Dec 5, 2021 3:55 AM UTC

Hi, to everyone who looked here I eventually found the solution.

In the usbd_cdc_if.c file had to add this code :

1
 /* USER CODE BEGIN INCLUDE */
#define APP_RX_DATA_SIZE 2048// !!! aded by me
#define APP_TX_DATA_SIZE 2048
/* USER CODE END INCLUDE */
 2 
/* Private variables ---------------------------------------------------------*/
uint8_t buffer[7]; //!!!!!!Added by me
/* USER CODE END PV */
 3 
case CDC_SET_LINE_CODING:
 		 buffer[0]=pbuf[0]; //////////Added by me
 			buffer[1]=pbuf[1];
 	 	 	buffer[2]=pbuf[2];
 	 	 	buffer[3]=pbuf[3];
 	 	 	buffer[4]=pbuf[4];
 	 	 	buffer[5]=pbuf[5];
 	 	 	buffer[6]=pbuf[6];
 
 break;
 
 case CDC_GET_LINE_CODING:
 			pbuf[0]=buffer[0];
 	 	 	pbuf[1]=buffer[1];
 	 	 	pbuf[2]=buffer[2];
 	 	 	pbuf[3]=buffer[3];
 	 	 	pbuf[4]=buffer[4];
 	 	 	pbuf[5]=buffer[5];
 	 	 	pbuf[6]=buffer[6];
static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
 /* USER CODE BEGIN 6 */
 USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
 USBD_CDC_ReceivePacket(&hUsbDeviceFS);
 CDC_Transmit_FS(Buf, *Len); // ADED BY ME !!!!!!!!!!!!!
 return (USBD_OK);
 /* USER CODE END 6 */
}

and this solves the problem.

Moderator you can consider this problem closed.