Skip to main content
Dariush.Tsh
Associate III
September 29, 2021
Solved

Is the SPC5-HTCOMP-NLTL compiler free or should it be purchased? If so, what is the price and from which source should it be purchased? Also please tell us more about this SPC5-HTCOMP-NLTL.

  • September 29, 2021
  • 1 reply
  • 937 views

..

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    The SPC5-HTCOMP-NLTL compiler has been obsolete for several years.

    Instead, however, you can use SPC5_STUDIO, which can be equipped with multiple compilers, e.g. the free licensed GNU GCC Compiler, the Greenhills Compiler (license required) or the GNU C Compiler from HighTec EDV-System (license required).

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    1 reply

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    September 29, 2021

    The SPC5-HTCOMP-NLTL compiler has been obsolete for several years.

    Instead, however, you can use SPC5_STUDIO, which can be equipped with multiple compilers, e.g. the free licensed GNU GCC Compiler, the Greenhills Compiler (license required) or the GNU C Compiler from HighTec EDV-System (license required).

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.