[SMT32CubeIDE] v1.70 Cannot create a new project
I have downloaded the latest version of the STM32CubeIDE.
Version: 1.7.0
Build: 10852_20210715_0634 (UTC)Integrated STM32CubeMX version:
STM32CubeMX - STM32 Device Configuration Tool
Version: 6.3.0-RC5
Build: 20210714-1111 (UTC)
Copyright (c) 2021 STMicroelectronics. All rights reservedHowever, I am not able to create a new project.
I get the following error. I never had to install anything separately before.
Update:
I installed CubeMX (v6.3.0) to generate the initial IOC file and that went fine.
On opening the IOC file (after setting up the project with said IOC file), the kernel seems to have crashed (notification on startup) and my system just shut down.
I am using fedora 34.