Skip to main content
SGasp.1
Associate III
Jul 17, 2021 7:34 PM UTC
Question

Update external flash memory via usb stick

I have developed a custom bootloader for updating the fw via usb stick for stm32F7...I would like to integrate the possibility to update the external flash memory via quadspi... Which are the adds what I should introduce to the initial bootloader in order to update the external memory? Is it enough to add the quadspi connectivity in the ioc project and then import two files (quadspi_cmd.h and quadspi_cmd.c) and after reading the content of the usb stick call the routine CSP_QSPI_WriteMemory? Thanks a lot for your kind support

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jul 17, 2021 11:27 PM UTC

Personally, I'd probably merge in the pin stuff from one of the DISCO/EVAL type BSP, changing the pin assignments in the MSP code.

The CSP stuff here looks like you should be able to take it at a file level. Write is decomposed into page size chunk so that shouldn't need any additional work.

Might want to take a look at the External Loader examples to understand how this interacts with the CSP layer, but it looks reasonably clean / straight forward.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..