ISSUE with STSAFE_Provisioning project in X-cube_AWS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-13 7:01 AM
hi i am trying to run AWS_DEMOS project on b-l4s5i-iot01 board. i build stsafe_provisioning project but got the error mentioned below after the programming the image.
i could use some help. build doesn't throw any errors. and i haven't changed anything in the source code. x-cube-aws(2.0.0)
Start provisioning of STSAFE-A
Force STSAFE-A provisioning
Launching STSAFE-A provisioning
Check if Pairing Host keys available
Provisioning OK
Erase Data : NOK !!!!
Now Store Certificate STM_POC_SBSFU_ROOT_TEST_CA_00 inside STSAFE
Store Data NOK !!!!
Now Store Data using HAL_Store_Data
Now Store Certificate STM_POC_SBSFU_OEM_TEST_CA_00 inside STSAFE
Store Data NOK !!!!
End provisioning of STSAFE
Store Data NOK !!!!
Now Store Data using HAL_Store_Data
Now Store Certificate STM_POC_SBSFU_OEM_TEST_CA_00 inside STSAFE
Store Data NOK !!!!
End provisioning of STSAFE
- Labels:
-
STM32CubeExpansion
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-30 3:07 AM
Hi,
a possible source of error is the flash bank configuration of the STM32L4S5 MCU.
It is set in the DBANK option, which can be edited by the STM32CubeProgrammer tool.
X-CUBE-AWS v2.0.0 requires that the DBANK option is enabled (= dual bank).
X-CUBE-AWS v2.1.x and v2.2.x require that the DBANK option is disabled (= single bank).