cancel
Showing results for 
Search instead for 
Did you mean: 

Antenna Specifications provided along with ST25RU3993-HPEV kit as accessories.

Prabhu1
Associate II

As per the latest product brief DB4247 Rev 3 (May 2021) it says the accessories list containing PCB and Patch Antenna.

Where I can find specification of the both the antenna (Gain, Bandwidth, EU/USA details)

Data brief - ST25RU3993-HPEV - RAIN® (UHF) RFID reader evaluation kit

Please share the list for better understanding to configure the transmit power.

regards

Prabhu

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Dear SKann.1,

the included patch antennas are:

1 x SlimLine A5020 FCC variant from Times-7

1 x SlimLine A5020 ETSI variant from Times-7

The PCB Near-Field antenna is a STM custom built antenna

  • VSWR: 1.2 (typical)
  • no far field (Gain < -20 dB)
  • magnetic field is concentrated in the center of the antenna (see image)0693W00000CzoPuQAJ.png

The transmit power of the reader can be adjusted in the GUI.

Please refer to the GUI user manual for more information.

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

Dear SKann.1,

the included patch antennas are:

1 x SlimLine A5020 FCC variant from Times-7

1 x SlimLine A5020 ETSI variant from Times-7

The PCB Near-Field antenna is a STM custom built antenna

  • VSWR: 1.2 (typical)
  • no far field (Gain < -20 dB)
  • magnetic field is concentrated in the center of the antenna (see image)0693W00000CzoPuQAJ.png

The transmit power of the reader can be adjusted in the GUI.

Please refer to the GUI user manual for more information.

Cheers,

B