Skip to main content
RZieb
Associate
June 28, 2021
Solved

STM32F746IGT - Cannot trigger ADC conversion with Timer 4

Hello,

I'm working on hobby project using STM32F746IGT. I wrote ADC init sequence but cannot get it working properly. Timer 4 reloads at given period and It's interrupt is called properly. ADC starts conversion after setting SWSTART bit manually but I cannot make Timer4 to trigger ADC1.

Please help :)

void adc_init( void )
{
	RCC -> APB2ENR |= RCC_APB2ENR_ADC1EN;
	RCC -> APB1ENR |= RCC_APB1ENR_TIM4EN;
	RCC -> AHB1ENR |= RCC_AHB1ENR_GPIOAEN | RCC_AHB1ENR_GPIOHEN;
 
	gpio_pin_cfg(GPIOA, 7, GPIO_ANALOG);
 
	// Timer 4 TRGO
	// Max 36 MHz @ 3.3V
	ADC->CCR = ADC_CCR_ADCPRE_0 | ADC_CCR_ADCPRE_1;
 
	ADC1->CR2 = ADC_CR2_EXTEN_0 | ADC_CR2_EXTSEL_3 | ADC_CR2_EXTSEL_2 | ADC_CR2_ADON;
	ADC1->CR1 = ADC_CR1_SCAN | ADC_CR1_DISCEN | ADC_CR1_EOCIE;
	ADC1->SQR1 = 0; 				// 1 regular conversion
	ADC1->SQR3 = (7 << 0); 		// 1st conv IN7
	ADC1->SMPR2 = (0b001 << (7*3)); // IN7 112 cycles
	NVIC_EnableIRQ( ADC_IRQn );
	NVIC_EnableIRQ( TIM4_IRQn );
 
	ADC1->CR2 |= ADC_CR2_SWSTART;
 
	// Sampling 16000 Hz
	//
	TIM4 -> ARR = 125 - 1;
	// 500ns tick
	//
	TIM4 -> PSC = 216/2/2 - 1;
	TIM4 -> CNT = 0;
	TIM4 -> EGR = TIM_EGR_UG;
	TIM4 -> CR2 = TIM_CR2_MMS_1;
	TIM4 -> DIER = TIM_DIER_UIE;
	TIM4 -> CR1 |= TIM_CR1_CEN;
}
 
 
void ADC_IRQHandler(void)
{
	ADC1->SR = 0;
	ADC->CSR = 0;
	//static uint8_t val = 0;
	double in = (double)(ADC1->DR-2048.0)/4096.0;
	in++;
}
 
void TIM4_IRQHandler(void)
{
	TIM4->SR = 0;
}

This topic has been closed for replies.
RZieb
RZiebBest answer
Associate
June 29, 2021

According to Erratasheet enabling DAC (!) clock is mandatory to get TRGO signal working:

RCC -> APB1ENR |= RCC_APB1ENR_DACEN;

It would be much easier for developers if they have placed that piece of information in ADC paragraph ;)

11 replies

waclawek.jan
Super User
June 28, 2021

Looks OK.

SCAN and DISCEN are maybe redundant, but shouldn't make harm, similarly TIMx_DIER and clearing ADC_CSR (which is a read-only copy of the individual status registers).

Try to read out and check content of both TIM and ADC registers, maybe observing the status register(s).

JW

RZieb
RZiebAuthor
Associate
June 29, 2021

Thank you for your response.

Unfortunately every flag in registers seems OK. Probably there are some hardware issues with internal TRGO matrix.

RZ

RZieb
RZiebAuthorBest answer
Associate
June 29, 2021

According to Erratasheet enabling DAC (!) clock is mandatory to get TRGO signal working:

RCC -> APB1ENR |= RCC_APB1ENR_DACEN;

It would be much easier for developers if they have placed that piece of information in ADC paragraph ;)

TDK
June 29, 2021

What a bizarre requirement. Thanks for reporting. Sure enough, that's exactly what Cube examples do. Wonder if generated code would do the same as well.

https://github.com/STMicroelectronics/STM32CubeF7/blob/c7c5ec99c7482ea8bcdbf0a869c930af4547088f/Projects/STM32756G_EVAL/Examples/ADC/ADC_TriggerMode/Src/main.c#L94

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
June 29, 2021

> Sure enough, that's exactly what Cube examples do.

Oh, between steps 4 and 3 (in this order). Without a single line of explanation. Very characteristic.

JW

waclawek.jan
Super User
June 29, 2021

Kudos for finding this.

Thanks for coming back with the answer. Please select your post as Best so that the thread is marked as Solved.

JW

waclawek.jan
Super User
February 17, 2023

> CubeMX generated code does not enable the DAC clock. I'm sure that will burn someone in the future.

It did.

https://community.st.com/s/question/0D53W000028TMnYSAW/stm32f746-adc3-does-not-work-with-external-trigger-from-timer

@Amel NASRI​ , can you please have a look at this?

Thanks,

JW

Amel NASRI
ST Technical Moderator
February 22, 2023

Thanks @Community member​ for coming back to this discussion. As confirmed here, issue is tracked internally.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
waclawek.jan
Super User
February 22, 2023

Thanks, Amel.

Jan