Solved
Default HSI Calibration Value wrong in STM32CubeIde
Hello,
I am using the STM32L412, when I activate the HSI clock in the .ioc, HSI Calibration Value is set to 16 (0x10).
Looking at stm32l4xx_hal_rcc.h:
#if defined(RCC_ICSCR_HSITRIM_6)
#define RCC_HSICALIBRATION_DEFAULT 0x40U /*!< Default HSI calibration trimming value 64 on devices other than STM32L43x/STM32L44x/STM32L47x/STM32L48x */
#else
#define RCC_HSICALIBRATION_DEFAULT 0x10U /*!< Default HSI calibration trimming value 16 on STM32L43x/STM32L44x/STM32L47x/STM32L48x devices */
#endif /* RCC_ICSCR_HSITRIM_6 */So, with STM32L412, the default value set by the device configuration tool should be 60 (0x40).
With default value USART was failing, once changed everything was working good for me.