Skip to main content
SJain.3
Visitor II
May 24, 2021 4:20 AM UTC
Question

H2PAK-2 vs H2PAK-6 MOSFET package for high current application

I'm using multiple MOSFET of STH310N10F7 in parallel for current of approximately 60A.

MOSFET are used in DC Bias and not switching so time delay is not a factor of consideration.

I'm confused between the packages.

What are intended application of H2PAK-2 vs H2PAK-6 package? Which is suggested for pure DC bias application?

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    May 25, 2021 9:23 AM UTC

    H2PAK-2 is fully compatible with the D2PAK footprint, making it easy to upgrade.

    H2PAK-6 offers some advantages in passing the low Rdson to the board.

    The chip inside and parameters are identical, so both can be used for the same application.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.