L6599AT gate drive pulses appear unexpectedly
We noticed that there are pulses at the gate drive outputs (pins 15 HVG, & 11 LVG) during the ramp-up of the control voltage (pin 12 VCC).
This is what we saw: when VCC reaches about 11V, a sequence of pulses appear on both LVG and HVG. First LVG went high (VCC) for a long period of about 10 micro-seconds, then it went low, and after a delay of about 300ns, 3 narrow pulses (each less than 250ns wide) appeared alternately on both HVG and LVG, in normal sequence with deadtime of about 300ns, starting with HVG first, and the last pulse on LVG. Then the pulses stop for a very long period (many hundreds of milli-seconds), and then they start again in accordance with the normal function of the controller in response to voltages at the control pins. The behaviour occurred regardless of the rate of rise of VCC, we varied this from very fast (2 milli-seconds rise from 0V to +12V) to quite slow (100ms from 0V to +12V) and each time the response was the same.
We also saw pulses on the timing cap, pin 3 CF. This voltage was held at 0V during VCC ramp, then held at about 0.5V for the first pulse (LVG high for 10us), then it showed the usual triangle waveform for 3 peaks and 3 valleys during the narrow pules on LVG & HVG, then it returned back to 0V.
During the time of these unexpected pulses (during the ramp of VCC) all of the inputs are set to voltages that would normally cause gate drivers to both stay at 0V. To be specific, these are the voltages at the control pins during the ramp-up time of VCC and during the time when these pulses occur:
Pin 2 TripDelay is at 0V.
Pin 5 STBY is at 0V.
Pin 6 ISEN is at 0V.
Pin 8 Disable is at 0V.
Pin 4 is at 2V (as expected). Note that the current out of this pin is at maximum, since the control voltage is at 0V (refer datasheet figure 22, this is equivalent to the opto Q being fully ON) - this would normally cause the Fs to be a minimum (maximum output power), but at this time the chip is being held in the shutdown state by pin 5 and pin 1 (Soft-start) is at 0V, which should be forcing Fs to be very high.
So to summarise: during VCC ramp up, our circuit keeps the pins of the chip in the states necessary to prevent any pulses appearing on LVG & HVG, yet we are seeing pulses. This leads me to suspect that this behaviour is built into the chip itself, and is beyond our control. But I have not seen any mention of this behaviour in any datasheet, or app note, and I looked in this forum but could not find any mention of it.
I have attached some waveforms that show this.
Please respond to the following questions:
Q1. Is this behaviour normal?
Q2. is any way to prevent these pulses from occurring?
Q3. Does this behaviour occur for all the different variants of this chip?
Q4, Does this behaviour also occur for the new chip, the L6699?
Regards,
-F.Barone.
Scope images below:
CH1 +12VA (Vcc)
CH2 XAB
CH3 pin 4 RFmin
CH4 pin 3 CF
Scope images below:
CH1 same, +12VA (Vcc)
CH2 same XAB
CH3 moved to pin 11 LVG
CH4 moved to pin 15 HVG