Skip to main content
Ted Jackson
Senior
April 8, 2021
Solved

In STM32CubeIDE, how does one determine the 'Core Clock' and 'SWO Clock' rate in the Debug Configuration for a working project from source and no IOC file?

  • April 8, 2021
  • 5 replies
  • 5129 views

..

This topic has been closed for replies.
Best answer by Tesla DeLorean

 printf("\n\nCore=%d, %d MHz\n", SystemCoreClock, SystemCoreClock / 1000000);

The SWO side clock is usually determined by the debugger side interface, ie 2 MHz or whatever, and it then programs the chip side SWO baud rate and encoding scheme to relate the two. ie divisor = (168000000 / 2000000) - 1

The H7 side code looked like this

//SWO current output divisor register

//This divisor value (0x000000C7) corresponds to 400Mhz

//To change it, you can use the following rule

// value = (CPU Freq/sw speed )-1

*(__IO uint32_t*)(0x5C003010) = ((SystemCoreClock / 2000000) - 1); // SWO_CODR

Other systems

TPI->ACPR = ((SystemCoreClock / 2000000) - 1); /* "Async Clock Prescaler Register". Scale the baud rate of the asynchronous output */

5 replies

Tesla DeLorean
Guru
April 8, 2021

You look at the clock and PLL settings

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ted Jackson
Senior
April 8, 2021

I see no mention of Core Clock or SWO Clock in SystemClock_Config() or in a typical Clock Configuration page in CubeMX. Is there no utility to just measure that resultant clock rate? Can you be more specific please?

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
April 8, 2021

 printf("\n\nCore=%d, %d MHz\n", SystemCoreClock, SystemCoreClock / 1000000);

The SWO side clock is usually determined by the debugger side interface, ie 2 MHz or whatever, and it then programs the chip side SWO baud rate and encoding scheme to relate the two. ie divisor = (168000000 / 2000000) - 1

The H7 side code looked like this

//SWO current output divisor register

//This divisor value (0x000000C7) corresponds to 400Mhz

//To change it, you can use the following rule

// value = (CPU Freq/sw speed )-1

*(__IO uint32_t*)(0x5C003010) = ((SystemCoreClock / 2000000) - 1); // SWO_CODR

Other systems

TPI->ACPR = ((SystemCoreClock / 2000000) - 1); /* "Async Clock Prescaler Register". Scale the baud rate of the asynchronous output */

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..