Skip to main content
CLi.4
Associate
Apr 7, 2021 9:43 AM UTC
Question

RT-Thread Studio IDE V2.1.0 Release to Better Support STM32 Development!

RT-Thread Studio IDE has the features of project creation and management, code editing, SDK manager, build configuration, debug configuration, program download and debugging, and combined with graphical configuration systems and package and component resources. RT-Thread Studio engaged to offer developers a handy IDE so that can reduce repetitive work, minimize the difficulty of project development, improve work efficiency both in speed and quality, and accelerate the overall product development process.

Highlights:

1-Support Different Project Creation Wizards:

Supports the bare board project creation, RT-Thread-based project creation, and many other creation wizards, developers can create projects based on ST series MCU or the development board:

0693W000008yrMlQAI.png 

2-SDK Manager Supports ST All Series of MCUs and 40+ Dev Boards:

0693W000008yrIuQAI.png 

3-System Configuration Feature

RT-Thread configuration features include both framework configuration and tree configuration, where packages can be added through the Package Center and related components can be enabled directly by clicking on the component icon. Under the tree configuration interface, all configuration options can be configured directly. In addition, the configuration tree right-click menu has added a search function to facilitate the location of the target configuration items.

0693W000008yrOXQAY.png 

4-Easy-to-use Toolbar Buttons:

0693W000008yrOrQAI.png 

5-Support MDK Development

RT-Thread Studio v2.1.0 supports bilateral synchronous co-development with the MDK project. You can import an existing RT-Thread MDK project directly into RT-Thread Studio, and the configuration of the MDK will be automatically synchronized with the RT-Thread Studio project. RT-Thread Studio provides a bilateral synchronization mechanism that allows the project to switch between MDK and RT-Thread Studio at any time. The MDK configuration feature is also supported to perform configuration items such as C/C++, ASM, Linker and automatically synchronized with MDK projects when the configuration is completed. If you modify some configurations on the MDK, you can manually trigger synchronization at RT-Thread Studio to sync the modified configurations with RT-Thread studio projects.

For more details please check out here!

0693W000008yrP6QAI.png 

6-Support CubeMX Development

RT-Thread Studio v2.1.0 is also in collaboration with STM32CubeMX, where you can open CubeMX Settings directly in RT-Thread Studio. After configuration, click the button GENERATE CODE, and the code generated in CubeMX will automatically be copied into the RT-Thread Studio project directory, no further modifications are required. Then it is automatically added to the compilation. We only need to compile, download and debug programs as usual.

For more details please check out Here!

0693W000008yrQnQAI.png 

7-Support QEMU:

QEMU is a cross-platform simulator that supports many development boards. It is convenient to validate prototype development if you don’t have a development board and hardware debugger on hand. RT-Thread Studio provides direct support to QEMU simulation debugging which has the following features:

  • Create a project that uses the QEMU simulator by default
  • Visual configuration of QEMU command parameters
  • Simulate physical boards for breakpoint debugging
  • Supported dev boards:
  • STM32F407-ATK-EXPLORER
  • STM32F429-ATK-APOLLO
  • STM32F429-FIRE-CHALLENGER
  • STM32F429-ST-DISCO
  • STM32F401-ST-NUCLEO
  • QEMU-VEXPRESS-A9
  • STM32F410-ST-NUCLEO
  • GD32VF103-NUCLEI-RVSTAR

0693W000008yrPuQAI.png 

8-A Variety of Debuggers Are Supported

Supports commonly used hardware debuggers like JLINK, STLINK and CMSIS-DAP LINK, and supports a wide range of many other debugging functions. For example, terminal function, users can easily check out the chip core registers, peripheral registers, variables, expressions, assembly code and memory data, supports assemble instruction step mode, breakpoint management and so on!

0693W000008yrQ4QAI.png 

9-Black DevStyle Theme

0693W000008yrQTQAY.png 

10-Online Documentation and Video Tutorials

RT-Thread builds an online tutorial video center, which step-by-step guides you to get started using RT-Thread Studio. RT-Thread Club is also opened to developers to share their development experiences, ask questions, and get answered.

Download RT-Thread Studio V2.1.0

Ideas for RT-Thread Studio, talk with us.

    This topic has been closed for replies.

    2 replies

    ST Technical Moderator
    Apr 7, 2021 2:45 PM UTC

    Hello @CLi.4​ and welcome to the STM32 Community :)

    Your post is much appreciated :smiling_face_with_smiling_eyes:

    Thanks for sharing this IDE release and features !

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    CLi.4
    CLi.4Author
    Associate
    Apr 12, 2021 5:33 AM UTC

    Hi Imen. May we have this post pin in the ST community in exchange for the post of lighting up LED?