Skip to main content
MKılı.1
Associate
April 6, 2021
Question

Can I increase the flash memory of STM32G030K8T6 with SPI NOR Flash memory?

  • April 6, 2021
  • 4 replies
  • 1059 views

Hello,

I am trying to use a 240x320 ili9341 screen with g030 but even one picture doens't fit into flash memory. (If you are familiar with ILI9341, the picture I am talking about is snow_tiger)

I made some research on it and saw that in TouchGFX website  STM32G071 nucleo board with the X-Nucleo-GFX01M1 expansion board is used. The expansion board has 64-Mbit SPI NOR Flash memory.

If I buy a NOR Flash memory, can I overcome my problem?

Thank you

This topic has been closed for replies.

4 replies

MKılı.1
MKılı.1Author
Associate
April 6, 2021

I tried using SD Card but when I imported FATFS middeware on CubeMX, RAM overflowed :(

Tesla DeLorean
Guru
April 6, 2021

It doesn't provide for a QSPI interface, so can't be mapped into the processors memory space, or allow for Execute-In-Place.

SPI access should be viable, and have a relatively small code foot-print.

You could page data and code into RAM.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MM..1
Super User
April 6, 2021

You can add SPI memory, but with 8kB RAM i mean you waste time with 030 try work with graphics. Why not start with other?

MKılı.1
MKılı.1Author
Associate
April 9, 2021

Okay guys thank you for the answers