2021-04-05 6:51 AM
I want to use wake up interrupt for two different thresholds at the same time,
for example I want to give wake up threshold 1g for interrupt 1,
I want to give 500 mg for interrupt 2. And duration will be different.
I change the value of WAKE_UP_THS, WAKE_UP_DUR registers while configuring second interrupt.
Is it possible to do it ? How can I do it ?
2021-10-12 8:56 AM
Hi @Iakgu.1 ,
with a bit delay... is this question related to this other thread?
If so, can we close this one?
-Eleon