Skip to main content
ADres.2
Visitor II
March 31, 2021
Question

Glue which contains phthalates is used in IC. Percentage of phthalates (DBP) is exceeded allowed threshold level stipulated by EU RoHS directive. - Does the DBP evaporate during manufacturing process?

  • March 31, 2021
  • 0 replies
  • 547 views

Hi, I got material compliance from Silicon Expert Database. Concerned part is an IC. According to Silicon Expert, there is glue used for die attach. The glue contains a phthalate based substance, DBP. DBP use is restricted by EU RoHS directive, via delegated directive 2015/863. There shall be not more than 0,1% w/w of this phthalate in homogenous material in an EEE (i. e. in the IC which is integrated into an EEE). Problem: the glue contains more DBP than allowed by EU RoHS directive. It´s about 0,2 %, not 0,1 %. Actually, it´s mikrograms per IC. But it is exceeding the threshold. - QUESTION: What happens with DBP in such glue? Does it evaporate when the glue material hardens? I. e. is there no DBP remains in the IC when it is distributed? - I am grateful for helpful hints.

    This topic has been closed for replies.