STM32WB Low power manager
Hi everybody,
I'm a student in a French engineering school currently working on a project including the STM32WB wireless CPU series. For the sake of simplicity, I'm just going to say that my project basically consist in establishing a BLE connection using a 1000 µF capacitor as my only energy source.
Here comes my question : I've tried using the "Low power manager" that comes with the sequencer when generating the code trough CubeMx : I've enabled it in app_conf.h aswell as disabled all debugging options and made sure it was configured for the StopMode2. My understanding is that my STM32WB should enter StopMode between 2 advertising packets, so if I monitor the consumption , I should be able to see it drop to a couple µA when in StopMode and rising back up for a very short time everytime a packet is sent.
However, when configuring the advertising to send a packet every 5 secondes, my energy comsumption do not drop to a couple µA after sending the first packet. My guess is that i'm not actually entering StopMode but I can't figure out why.
Any help is greatly appreciated, sorry for my bad english.