cancel
Showing results for 
Search instead for 
Did you mean: 

DFU Mode STM32H7 saying " USB DEVICE NOT RECOGNIZED"

CLeo.1
Senior II

Hi guys, finally was able to pin VDD to VDDUSB33, re-tried it now the computer is at least detecting a device!

However, the software for the DFU is not able to pick up the device as the computer keeps saying "USB DEVICE NOT RECOGNIZED"

This is what I am saying in device manager 0693W000008y6DcQAI.jpg 

I have already installed the x64 drivers when you download the software set but still no prevail. Any ideas?

1 REPLY 1
Imen.D
ST Employee

Hello @CLeo.1​ ,

Can you specify which STM32CubeProgrammer are you using?

Please, make sure to use the latest release of STM32CubeProgrammer V2.7.0.

If possible to check that you have the same issue with different board.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen