How to know inner connections of DMA channels to peripherals on stm32g4 series mcu?
I have worked with f3 series and in user manual there is shown what peripherals are connected to each DMA channel. For example 4 peripherals are connected to one channel, that means I have to configure only one peripheral to use that DMA channel to serve this specific event, because channel configuration includes from which address to which move the data..
In g4 series I found DMAMUX router, it has 115 inputs from all peripherals and 16 outputs to DMA channels. And the question I have is - how to know which DMAMUX output will be triggered on specific input? (for example ADC1 and ADC2, what other inputs will trigger the same DMA channel?)
This is my first question on forum, plz don't be too judgemental.