STM32 UART DMA reception fails to update memory buffer from peripheral
Hello ST,
I'm using STM32H743ZI. Here I'm connected to 2 external devices(1 for PC UART5 and other for another MCU UART7), both are connected via UART.
I'm using DMA with UART7 for receiving data from MCU. UART5 which we use to communicate with PC(Master) sends out some command, based on this command I request some data from MCU-UART7.
So when I receive data from PC, I'll continue to remain in UART5 ISR. In this ISR only we communicate with MCU continuously. When I receive command from PC, I send request to MCU to get back some data as response,
when MCU responds back I wanted to collect that data using UART7-DMA.
This is basic concept.
Now problem I'm facing is,
When I request for data to MCU, first time I get correct data loaded into my buffer through DMA(where it triggers both half and full complete IRQs) but second time onwards it doesn't update my buffer.
Whenever I receive data from MCU, I send that to PC-UART5. When again PC sends command and I again request data to MCU, it fails to update my buffere but still half and full IRQs are triggered.
What could be problem here? I tried to reinitialise UART and DMA everytime I request data from MCU, that didn't work.
I'm really stuck here, any help here will be very useful.
Code snippet looks something like below
static void MX_UART5_Init(void)
{
/* USER CODE BEGIN UART5_Init 0 */
// This UART is towards PC
/* USER CODE END UART5_Init 0 */
/* USER CODE BEGIN UART5_Init 1 */
huart5.RxISR = &UART5_InterruptCallback;
/* USER CODE END UART5_Init 1 */
huart5.Instance = UART5;
huart5.Init.BaudRate = 115200;
huart5.Init.WordLength = UART_WORDLENGTH_8B;
huart5.Init.StopBits = UART_STOPBITS_1;
huart5.Init.Parity = UART_PARITY_NONE;
huart5.Init.Mode = UART_MODE_TX_RX;
huart5.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart5.Init.OverSampling = UART_OVERSAMPLING_8;
huart5.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart5.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart5.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_DMADISABLEONERROR_INIT;
huart5.AdvancedInit.DMADisableonRxError = UART_ADVFEATURE_DMA_DISABLEONRXERROR;
if (HAL_UART_Init(&huart5) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart5, UART_TXFIFO_THRESHOLD_8_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart5, UART_RXFIFO_THRESHOLD_8_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart5) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN UART5_Init 2 */
HAL_NVIC_SetPriority(UART5_IRQn, 5, 5);
HAL_NVIC_EnableIRQ(UART5_IRQn);
__HAL_UART_ENABLE_IT(&huart5, UART_IT_RXFNE);
/* USER CODE END UART5_Init 2 */
}
/**
* @brief UART7 Initialization Function
* @param None
* @retval None
*/
static void MX_UART7_Init(void)
{
/* USER CODE BEGIN UART7_Init 0 */
// This UART is towards Nebo
/* USER CODE END UART7_Init 0 */
/* USER CODE BEGIN UART7_Init 1 */
huart7.RxISR = &HAL_UART_RxCpltCallback;
/* USER CODE END UART7_Init 1 */
huart7.Instance = UART7;
huart7.Init.BaudRate = 2500000;
huart7.Init.WordLength = UART_WORDLENGTH_8B;
huart7.Init.StopBits = UART_STOPBITS_1;
huart7.Init.Parity = UART_PARITY_NONE;
huart7.Init.Mode = UART_MODE_TX_RX;
huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart7.Init.OverSampling = UART_OVERSAMPLING_8;
huart7.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_ENABLE;
huart7.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart7) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart7, UART_TXFIFO_THRESHOLD_8_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart7, UART_RXFIFO_THRESHOLD_8_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart7) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN UART7_Init 2 */
HAL_NVIC_SetPriority(UART7_IRQn, 4, 4);
/* USER CODE END UART7_Init 2 */
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
}
Inside UART5 ISR, I request data from UART7 something like below
HAL_UART_DeInit(&huart7);
HAL_UART_Init(&huart7);
(void)HAL_UART_Receive_DMA(&huart7, &encoder_buffer[0], (uint16_t)11);
Will be waiting for response, Thanks in advance
@STM32H743_User
@STM32Techie
@Human_STM32
@Paul STM32_
@Tilen MAJERLE
@Community member
@Community member
@TDK
@Community member
@JoniS
@Piranha
@BSang