Skip to main content
Soner
Associate
March 24, 2021
Question

Often in transparent areas, in random locations, false pixels can appear. can cause such a problem?

  • March 24, 2021
  • 4 replies
  • 1408 views

attached video.

STM32F429

TFT 1024x600

This topic has been closed for replies.

4 replies

Alexandre RENOUX
Visitor II
March 25, 2021

Hello Sozde.1,

Do you have the same issue on the simulator ? Also can you try see what is invalidated when running the simulator ? (press F2 when the simulator is running)

F429 is not powerful enough to be used efficiently with huge display like 1024x600. I don't know if it could have an impact in your case but it's important to take that into account.

Your display is an LTDC display ? Please provide more information about your current setup (software versions, board, external flash, external ram, etc.)

/Alexandre

Soner
SonerAuthor
Associate
March 25, 2021

Dear Alexandre,

simulator works normally.

I did not observe any changes with the F2 key.

We use our own coreboard.

CPU STM32F429IET

SRAM IS42S16400J-7TLI

FHASH M29W256GL70N6

TFT ‎NHD-10.1-1024600AF-ASXV#-CTP-ND‎ 10.1" TFT w/CAPTOUCH

We used it on a 7 inch screen (800x480) before. there was no problem.

We are currently planning to test with STM32F746IET.

we couldn't understand my hardware or software problem!

What do you recommend. thanks.

Soner
SonerAuthor
Associate
March 25, 2021

Keil v5.29 (ARM Compiler v5.06 update 6 (build750)

TouchGFX Designer 4.15.0

Alexandre RENOUX
Visitor II
March 29, 2021

Hello Soner,

Did you check your clocks ? What's your display clock speed ? Are your framebuffers in external SRAM ? What's the bandwidth of this SRAM ? Same for Flash.

I suspect your clock frequencies are two low and the bandwidth is limited.

/Alexandre