Out-of-spec temperature behavior of STM32F412 (hard fault) ?
Hi all,
I am testing product samples fitted with STM32F412RET6 which has a temperature operating range of -40°C +85°C.
On some samples tested inside a climate chamber, the MCU unexpectedly reset due to cold temperature within operating range (e.g. -5°C).
I have reproduced this behavior with a freeze spray and used the debugger to see what really happens.
When abruptly cooled with the spray, some MCUs issue a hard fault. Those are the same that fail inside the chamber.
The faults don't seem to originate from a certain spot in the code.
It really seems that the chips are involved as I have unsoldered, resoldered and switched two chips (one good and one bad) and the problem followed the chip.
The firmware is the same as the chip revision.
Did you ever experience something similar ?