Skip to main content
JayDev
Senior
March 19, 2021
Question

Low Power Application Question

  • March 19, 2021
  • 5 replies
  • 2056 views

Hello everyone!

I had an application that was originally designed to run on a STM32WB55 but found it didn't have the resources we needed for it. The STM32MP1 seems like it has the potential to be a good fit for us as we could do the sensor processing on the M4 and some of the higher level calculations on the A7.

Our plan was to have the chip asleep until it received a wakeup signal from a sensor and then most the code was running from the M4. Once it had completed its data collection, it would do the processing from the A7.

We're still in the planning phase (to determine if this is the right processor for this application) but the issue I'm having trouble navigating is the low power modes. Below are some of the questions I have:

1) If I'm having code running on the M4, is it possible to put the A7 into a low power mode (like standby or stop)? I believe this would be possible according to page 134 of the datasheet (which seems to show this capability).

2) What is the recommended mode to run on the A7 so that I don't need to boot the system from scratch on wakeup? Or would all of the modes be able to wake up and resume? Is this what the "data retention" refers to?

3) Is it possible to wakeup only the M4 core rather than the A7 or does the A7 core have to be woken up to wake the M4?

Any help you can give me would be greatly appreciated. Thanks!

This topic has been closed for replies.

5 replies

PatrickF
ST Employee
March 22, 2021

Hi,

Note that the capabilities are linked to HW, but also to Linux SW. I think for your case, you could use LPLV-Stop, which ensure fast M4 wakeup from GPIO/EXTI while having minimal power from Linux. If power is a concern, Standby is possible, but with more constrains (e.g. longer wakeup times, Only RETRAM retained for M4, need to use WKUP pins).

Note that in all cases, the DDR power in self-refresh must be added in your platform power (as well as all external components as usual).

I recommend that you start by reading https://wiki.st.com/stm32mpu/wiki/How_to_define_your_low-power_strategy.

You could probably find many useful data in the other wiki pages.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
JayDev
JayDevAuthor
Senior
March 22, 2021

This is a great page, hadn't seen that one before! I'll have to read some of the other pages linked, seems like there's a lot of good info here! So, if I am reading this correctly:

1) Each of the modes mentioned don't require a cold boot and it is able to wake up from these states without the 30s bootup time that normally comes with booting linux?

2) It sounds like the RETRAM is specific to the M4? If so, that makes sense (and seems to be what this page suggests).

One additional question I had had more to do with the RAM itself (let me know if I should open a separate ticket). The description of the RAM was a bit more complicated than that of the STM32WB55 (which makes sense as this has a uC and a uP sharing resources). It describes the RAM situation of the STM32MP157A (which is what is used with the DK1 board, which is what we'll be starting with) as:

708 Kbytes of internal SRAM: 256 Kbytes of AXI SYSRAM + 384 Kbytes of AHB SRAM + 64 Kbytes of AHB SRAM in Backup domain and 4 Kbytes of SRAM in Backup domain

It was harder for me to understand what will be available for the M4 (where most our processing will be). I decided to build a simple project and take a look at the resources available (to make sure we have at least 256 kb of RAm to work with so we can port a good chunk of code over from the WB55. When I looked at the resources available, i was a bit confused:

0693W000008xcgoQAA.jpgI'm not sure how the above description correlates to the current settings. Is the RAM configuration customizable to I can allocate more RAM to the M4? if so, is this something that's done in the IDE or would I make the changes in the linker file?

I was able to find this on that page you sent me (once again, thanks for that, great reference!)

0693W000008xchDQAQ.jpgIt does look like it should have 384 kb of SYSRAM, which I believe would be the equivalent of what I was using with the WB55. I'm looking through the IDE and the reference guide and I'm not really putting the pieces together of how it's configured or how the above settings in the IDE correlate with the diagram above. How do the above IDE settings correlate with the 384 kB of SYSRAM? Is the IDE setup with only 128 kb of SYSRAM by default (RAM1_data) and I need to change the linker files of the M4 to allocate more? Also, what is "flash_text" and "ram2_ipc_shm"?

I apologize if these are really basic questions, this is my first time using a chip with a coprocessor and shared resources.

Thanks for your help!

PatrickF
ST Employee
March 23, 2021

Hi, you already find most of your information.

On OpenSTLInux, SYSRAM and DDR are reserved for A7 side,

For Cortex-M4, you have 384K+64K available for code, constant and data.

see https://wiki.st.com/stm32mpu/wiki/STM32MP15_RAM_mapping#Zoom_in_the_Cortex-A7-2FCortex-M4_shared_memory for details, as some areas could be reserved for Linux DMA buffers and Interprocess buffers.

"xx_text" is your code/constant area (mostly SRAM1/SRAM2), and "***_ipc_shm" is the interprocess buffers, see also https://wiki.st.com/stm32mpu/wiki/Linux_RPMsg_framework_overview

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent