Question
About alternate function of STM32F746
Hello,
STM32F74xxx Reference manual (RM0385) 6.3.2 I / O pin alternate function multiplexer and mapping has the following description.
After reset the multiplexer selection is alternate function 0 (AF0).
I think that when AF0 is selected, it will be assigned to the following functions.
After resetting these pins, will the clock be output until the initial setting of the register is completed?
PA8 is assigned to MCO1.
PC9 is assigned to MCO2.
Goto