Skip to main content
FBald.1
Associate II
March 17, 2021
Question

Hello, I used your example to configure the LIS2DS12, in single TAP mode, but the INT1 pin always remains high even when reading the TAP_SRC register. Could you give me some suggestions of what is missing in the configuration?

  • March 17, 2021
  • 1 reply
  • 1080 views

Single-tap example

Hereafter an example code which implements the SW routine for single-tap detection.

1. Write 60h in CTRL1

// Turn on the accelerometer

// ODR = 400 Hz, FS = ±2 g

2. Write 38h in CTRL3 // Enable tap detection on X, Y, Z-axis

3. Write 09h in TAP_6D_THS // Set tap threshold

4. Write 06h in INT_DUR // Set quiet and shock time windows

5. Write 00h in WAKE_UP_THS // Only single tap enabled (SINGLE_DOUBLE_TAP = 0)

6. Write 40h in CTRL4 // Single-tap interrupt driven to INT1 pin

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    March 17, 2021

    Hi @FBald.1​ ,

    I suggest you to consider the C implementation of the "Single Tap" feature on Github --> lis2ds12_tap_single.c

    This code implements not only the configuration, but also the main loop for the interrupt management and clearing.

    Here below the detailed script:

    /* Main Example --------------------------------------------------------------*/
    void lis2ds12_single_tap_(void)
    {
     /* Initialize mems driver interface */
     stmdev_ctx_t dev_ctx;
     dev_ctx.write_reg = platform_write;
     dev_ctx.read_reg = platform_read;
     dev_ctx.handle = &SENSOR_BUS;
     
     /* Check device ID */
     lis2ds12_device_id_get(&dev_ctx, &whoamI);
     
     if (whoamI != LIS2DS12_ID)
     while (1) {
     /* manage here device not found */
     }
     
     /* Restore default configuration */
     lis2ds12_reset_set(&dev_ctx, PROPERTY_ENABLE);
     
     do {
     lis2ds12_reset_get(&dev_ctx, &rst);
     } while (rst);
     
     /* Set XL Output Data Rate */
     lis2ds12_xl_data_rate_set(&dev_ctx, LIS2DS12_XL_ODR_400Hz_HR);
     /* Set 2g full XL scale */
     lis2ds12_xl_full_scale_set(&dev_ctx, LIS2DS12_2g);
     /* Enable Tap detection on X, Y, Z */
     lis2ds12_tap_detection_on_z_set(&dev_ctx, PROPERTY_ENABLE);
     lis2ds12_tap_detection_on_y_set(&dev_ctx, PROPERTY_ENABLE);
     lis2ds12_tap_detection_on_x_set(&dev_ctx, PROPERTY_ENABLE);
     lis2ds12_4d_mode_set(&dev_ctx, PROPERTY_ENABLE);
     /* Set Tap threshold to 01001b, therefore the tap threshold is
     * 562.5 mg (= 9 * FS_XL / 2 5 )
     */
     lis2ds12_tap_threshold_set(&dev_ctx, 0x09);
     /* Configure Single Tap parameter */
     //lis2ds12_tap_dur_set(&dev_ctx, 0x0);
     lis2ds12_tap_quiet_set(&dev_ctx, 0x01);
     lis2ds12_tap_shock_set(&dev_ctx, 0x02);
     /* Enable Single Tap detection only */
     lis2ds12_tap_mode_set(&dev_ctx, LIS2DS12_ONLY_SINGLE);
     
     /* Wait Events */
     while (1) {
     lis2ds12_all_sources_t all_source;
     lis2ds12_all_sources_get(&dev_ctx, &all_source);
     
     /* Check if Single Tap events */
     if (all_source.tap_src.single_tap) {
     sprintf((char *)tx_buffer, "Tap Detected\r\n");
     tx_com(tx_buffer, strlen((char const *)tx_buffer));
     }
     }
    }

    Let me please know if you can find this code useful.

    -Eleon