CubeIDE 1.6: internal managed builder erratic when no C files changed and parallel build (bug report)
When building a managed project and parallel build is enabled, and stop on 1st error is unchecked, and changes are not in C files (in .h files or in link script) : build hangs for ~20 seconds at 13%. Then it often indicates successful completion without rebuilding C files affected by change in .h files (failure to detect dependencies) or does not re-link after change in link script.
To work around, I have to clean and do full rebuild in such situations.
How I reproduce it:
* Take a non-trivial, big enough project. Something with LwIP or RTOS and dozen of HAL files.
* Enable parallel build, no stop on 1st error, use internal builder.
* Do a clean build (should succeed)
* Then (A) make change in link script (for example change base address in flash) and build normally.
(B) make change in some .h file (LwIP or RTOS config or stm32h7xx_hal_conf.h). Build normally
Cube IDE 1.6 on Windows 10, upgraded from 1.5.1
MCU project target : STM32H753